cancel
Showing results for 
Search instead for 
Did you mean: 

Feature request: create pair of .c and .h files

Andrew Neil
Evangelist III

It is a very common practice the source files go in pairs: a .h file with the interface, and a .c file with the implementation.

This is acknowledged in CubeMX - which has an option to do exactly that:

AndrewNeil_0-1730989041590.png

 

But, with CubeIDE (in fact, Eclipse), it requires a 2-step process:

  1. New > Source File;
  2. New > Header File.

 

Feature Request: add an option to create a pair of files - .c and .h - in one go.

1 REPLY 1
Mahmoud Ben Romdhane
ST Employee

Hello @Andrew Neil ,

First let me thank you for posting.

I've escalated the request to the concerned team (under internal ticket number 195933).

Thanks.

Mahmoud