2022-04-27 2:31 AM
Once I connect my board(f746-disco), there is a disk in which FAIL.txt appears which contains "The interface firmware FAILED to reset/halt the target MCU". I have been getting this error since yesterday. I found a question asked this community, it was recommended to update STLink. However I did this, the problem is not solved. Moreover, I removed and re-installed CubeIDE, but the problem still continues. When I try to upload a code via Cube IDE, I got
"Error in final launch sequence:
Failed to start GDB server
Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (4) No device found on target."
What can I do? Please help me it is very very urgent, it is vital for me.
Thanks for your help.
2022-04-27 4:15 AM
Is the board powered correctly? (test with multimeter)
Did it stop working or it just never worked?
2022-04-27 11:06 AM
What does stop working mean? The power led is lighting, but I cannot upload code to board.
Which part/component should I measure on the board?
And thank you for your answer.
2022-04-27 11:31 AM
What changed/happened when it stopped working.
Check jumpers related to powering board and STM32 chip.
Check connectivity of SWD/JTAG pins, see jumpers or solder bridges.
Current measuring jumpers?
Option bytes or Read Out Protection, RDP2 ??
2022-04-28 12:13 AM
To check all these, I need to look at schematic, dont I?
I have no idea what happened to my board and it stopped working. I just wanted to use built-in microphone, I configured everything, then plug the board to my pc, but I see the text file on the disk :(.
2022-04-28 4:57 AM
Update:
I researched more on Google, and saw some suggestion to use ST-Link Utility. At first, I connect NRST pin to 3.3V, and then used erase chip on st-utility, after that I uploaded a code(.hex file) compiled on MBED studio. The code works when I connect NRST to 3.3v, but now ST-Utility cannot see my device.