2019-11-23 8:04 AM
I am not sure this belongs here, it could just as well be in MCU, but i believe it could be a configuration problem, so i put it here.
I am working on a project with Cube IDE. when I tried to compile for the first time, the build failed because of errors in the auto generated drivers. To fix this, I tried to delete all drivers and let MX import them again, but the error persisted.
The Error:
invalid type argument of '->' (have 'TIM_HandleTypeDef {aka struct <anonymous>}') stm32f1xx_hal_tim.h />Project</Drivers/STM32F1xx_HAL_Driver/Inc line 1222 C/C++ Problem
invalid type argument of '->' (have 'TIM_HandleTypeDef {aka struct <anonymous>}') stm32f1xx_hal_tim.h />Project</Drivers/STM32F1xx_HAL_Driver/Inc line 1229 C/C++ Problem
make: *** [Src/subdir.mk:73: Src/stm32f1xx_it.o] Error 1 >Project< C/C++ Problem
make: *** Waiting for unfinished jobs.... >Project< C/C++ Problem
The Code:
#define __HAL_TIM_SET_COUNTER(__HANDLE__, __COUNTER__) ((__HANDLE__)->Instance->CNT = (__COUNTER__))
/**
* @brief Get the TIM Counter Register value on runtime.
* @param __HANDLE__ TIM handle.
* @retval 16-bit or 32-bit value of the timer counter register (TIMx_CNT)
*/
#define __HAL_TIM_GET_COUNTER(__HANDLE__) ((__HANDLE__)->Instance->CNT)
/**
* @brief Set the TIM Autoreload Register value on runtime without calling another time any Init function.
* @param __HANDLE__ TIM handle.
* @param __AUTORELOAD__ specifies the Counter register new value.
* @retval None
*/
I have no clue what is wrong, and I don't want to manually fix it, because cubemx will overwrite it anyway
Solved! Go to Solution.
2019-11-24 2:40 AM
Solved, I was stupid. The call needs a pointer
2019-11-24 2:40 AM
Solved, I was stupid. The call needs a pointer