2023-08-17 5:35 AM - edited 2023-08-17 5:35 AM
Hello,
after upgrading from 1.12.1 to 1.13.1 I encounter the following problem when trying to download my (previously working fine) project onto STM32:
Any ideas?
regards
Herbert
Solved! Go to Solution.
2023-08-18 8:00 AM - edited 2023-08-18 8:03 AM
Hello @herbert ,
Thank you for posting this issue.
At first, try to check the proxy settings following these steps:
- Under Window --> Prefenrences--> Network Connexion, activate Native provider
- Under Window --> Prefenrences--> Firmware Updater, click on Check Connection
don't forget Apply and Close, if the connection works.
Could you, also, try to:
- Power off the target board
- Disconnect the ST-LINK JTAG USB cable
- Re-connect it t the ST-LINK JTAG USB cable
- Power on the target board
- Check the debug configuration settings, such as the SWD/JTAG interface
- Start the GDB server with different port number
I hope this will help!
Thanks,
Rim
2023-08-17 1:45 PM
Try reverting back to version 1.12.1, this problem may be related to the ST-link frequency above 1000kHz.
2023-08-18 8:00 AM - edited 2023-08-18 8:03 AM
Hello @herbert ,
Thank you for posting this issue.
At first, try to check the proxy settings following these steps:
- Under Window --> Prefenrences--> Network Connexion, activate Native provider
- Under Window --> Prefenrences--> Firmware Updater, click on Check Connection
don't forget Apply and Close, if the connection works.
Could you, also, try to:
- Power off the target board
- Disconnect the ST-LINK JTAG USB cable
- Re-connect it t the ST-LINK JTAG USB cable
- Power on the target board
- Check the debug configuration settings, such as the SWD/JTAG interface
- Start the GDB server with different port number
I hope this will help!
Thanks,
Rim
2023-08-28 3:44 AM
Hello @Rim LANDOLSI,
thanks, your tip to Check Connection with the Firmware Updater did set me to the right direction, as this also suggested to go to Help->Check for Target Selector Device Database Updates, which then did the trick for me and I was again able to connect to my STM32F411 board.
regards Herbert