2021-05-16 8:19 AM
Oscilloscope_SignalsGenerator example Not Loading the Kit. i got the Error like
Error in final launch sequence:
Failed to execute MI command:
load E:\\ST\\en.stm32cubeh7_v1-9-0\\STM32Cube_FW_H7_V1.9.0\\Projects\\STM32H735G-DK\\Demonstrations\\Oscilloscope_SignalsGenerator\\STM32CubeIDE\\Debug\\Oscilloscope_SignalsGenerator-STM32H735G-DK_OoB_V1.0.0.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load E:\\ST\\en.stm32cubeh7_v1-9-0\\STM32Cube_FW_H7_V1.9.0\\Projects\\STM32H735G-DK\\Demonstrations\\Oscilloscope_SignalsGenerator\\STM32CubeIDE\\Debug\\Oscilloscope_SignalsGenerator-STM32H735G-DK_OoB_V1.0.0.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load E:\\ST\\en.stm32cubeh7_v1-9-0\\STM32Cube_FW_H7_V1.9.0\\Projects\\STM32H735G-DK\\Demonstrations\\Oscilloscope_SignalsGenerator\\STM32CubeIDE\\Debug\\Oscilloscope_SignalsGenerator-STM32H735G-DK_OoB_V1.0.0.elf
Error message from debugger back end:
Load failed
Load failed
2021-05-18 5:23 AM
Hello @senthil ,
Which CubeIDE version are you using ?
I added the topic "STM32CubeIDE" to your question in order to increase its chance to be reviewed by our CubeIDE experts.
Hello @Markus GIRDLAND ,
Can you please help on this issue ?
Imen
2021-05-18 5:59 AM
STM32CubeIDE
Version: 1.6.1
Build: 9958_20210326_1446 (UTC)
2021-05-19 7:22 AM
Hello senthil!
First of all, the linker script is wrong. The flash address is set to 0x9080000 which should be 0x8000000. It's either a fault in the documentation or the example project.
From our testing it looks like the example project is configuring the power regulator into the wrong mode as well.
The error stems from this:
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
So, I will probably need to refer this along to @Amel NASRI . What is the correct power regulator configuration for an STM32H735G-DK? Seems to be different in MX generated project vs example projects... None work well?
2021-05-19 7:45 AM
Hi @senthil & @Markus GIRDLAND ,
Default configuration for STM32H735G-DK is SMPS mode. This is what we find in UM2679 Discovery kit with STM32H735IG MCU.
Being in a deadlock situation because of a mismatch between HW & FW setting for the power, it is required to follow the sequence described in the same user manual:
You can find some more details in this article as well: Unable to connect to STM32H7 devices.
-Amel
PS: PS: Once your question is answered, please click on "Select as Best" for the comment containing the answer to your initial question.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-05-19 8:40 PM
i follow your steps, still i am getting Same Error but other example folder Projects Working this Demonstrations Folder Projects Not working.
2021-05-20 2:07 AM
Hi @senthil,
I had a look at this. I think there are some mix-ups / copy-paste errors in this example project.
As @Markus GIRDLAND shared:
@Amel NASRI, can we have someone from CubeH7 do a proper analysis? Internal ticket references: 107323 + 107327 + 107329.
@senthil, as I said, no master of how this example should be working, so these are just some preliminary findings that may point you in the right direction. I will forward the issue internally to get some proper fixes.
2021-06-02 7:36 AM
@senthil,
Some follow-up: The three first bullets in my reply above has been fixed. More analysis on-going.
Something worth mentioning is that if you generate a new "STM32Cube project" inside CubeIDE or with stand-alone CubeMX, then there is an important bug fix for this board in MX-6.2.1 corresponding to IDE-1.6.1. This is with respect to the power regulator configuration. Using the previous version will "brick" the board (recoverable as described by Amel above).
2021-06-03 9:12 PM
I am Directly Open the Example Project in CubeIDE
STM32CubeIDE
Version: 1.6.1
Build: 9958_20210326_1446 (UTC)
OS: Windows 10, v.10.0, x86_64 / win32
Java version: 11.0.9.1
2021-06-04 2:24 AM
"I am Directly Open" ... please share snapshot of explain more "directly" .. there are numemous way to do ... my answer is depending of way :)