2019-10-22 2:58 AM
Hi,
after upgrading my STM32CubeIDE application to latest version 1.1.0 I'm unable to debug my project.
According to the log it seems that debugger is unable to identify my STM32F401RE anymore.
I tried with a new empty project and I encountered the same issue. Here following the output of the log:
STMicroelectronics ST-LINK GDB server. Version 5.3.2
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
Log output file: /tmp/STM32CubeProgrammer_7uowht.log
ST-LINK SN : 50FF71067788545428432167
ST-LINK FW : V2J34S7
Voltage : 3.19V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Cannot identify the device
Error: unknown or unsupported device (DevID = 0x0000)
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_V9fWXA.srec
File : ST-LINK_GDB_server_V9fWXA.srec
Size : 7328 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.056
Verifying ...
Error: Data mismatch found at address 0x08000004 (byte = 0x55 instead of 0xB1)
Error: Download verification failed
Encountered Error when opening /Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.macos64_1.1.0.201910081157/tools/bin/STM32_Programmer_CLI
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
2019-11-03 1:27 PM
Thank you ! I was just doing the "step-by-step" pdf and didn't't understand why the debug wasn't working, think I will install previous version instead.
2020-01-29 6:21 AM
29 Jan 2020: I've had a VERY SIMILAR experience: I've been using STM32CubeIDE alongside the separate STM32CubeProgrammer for a couple of months. I'm using BluePills (STM32F103) with the ST-LINK V2 JTAG/SWD programmer / ICE.
All the Edit-and-Compile territory seems to work fine, the programmer is on the button, and I've managed to educate myself about the suite while writing / compiling / burning and running several test programs. I gather this tool was previously TrueStudio by Atollic (is that correct ?) and that ST acquired them to build this "in-house" suite.
So far so good. Getting DEBUG to behave took a while -- the ST-LINK I have is fine, never seems to cause issue --- but the full STLINK-with-GDBServer experience I found fails instantly when the GDB server insists on checking the "ID" on the STM32 chip on the board -- this differs by one digit on the BluePills from the supposed ID code - and the GDB server will have no more of it and exits. BUT, up to now - the second option -- "ST-LINK OpenOCD" -- worked FINE, as that check appeared not to be made, and the whole step-through-code / stop and review memory content process, all worked fine, I was even starting to learn some GDB commands, as you get a GDB console still (not quite clear how / this is some alternate incarnation of the GDB service presumably, not made clear in the docs). All of that WORKED FINE all yesterday until..... suddently it didn't. Now, NOTHING: No debug functionality at all: IDE behaves exactly as before, except, when I hit the final "Debug" button in the Debug_Configuration options panel, which previously launched two consoles, one STLINK and one GDB and set off the whole debug cycle....
- ABSOLUTELY NOTHING happens - as if I had not touched the mouse.
So --- dug around looking at configs, could find nothing relevant. Ran a ps -ef | grep gdb and could see no GDB server running.... even if I switch back to the "ST LINK - GDB Server" option for debug. Something's not getting launched.
Battled with this for an hour / finally UNINSTALLED the whole STM32CubeIDE in toto using synaptic: REINSTALLED, all the way from the downloaded master script.
IDE back up.. EXACTLY THE SAME. NO Debug functionality at all. Test the ST LINK with CubeProgrammer --- works fine.
ST --- this is BRAND NEW V 1.2.0 IDE ST: downloaded clean and new a few days back (was using 1.0.2 before). What's going on ?
I thought this code was mature ?
Now I'm reading up on OpenOCD to learn if I can do all this OUTSIDE your IDE.
Might email this in to ST as well as the community to see what's afoot. I have WORK to do ST: tools should just work. I've put my trust in you -- waiting to buy silicon for products -- can you sort this out please ?