2021-04-13 07:54 AM
Hi
I have a global variable in the CUBE IDE's LIVE EXPRESSIONS window, I can see the values of my variablechaning. The values make sense. When I change the value manually, either the execution stops, the value is changed and I have to click on RESUME/F8 to continue debugging or the debugger detaches from target.
Is this a known issue?
I am using Segger Jlink via Jtag and/or SWD
2021-09-17 02:25 AM
I that case I use STMStudio to inject varaible value while is running application.
I'm trying to do the same but seem to don't works using STCubeIDE and STLink via SWD.
Regards
Maurizio Brignoli