2024-07-15 07:48 AM
How can I download my application onto board when debugging from the Cube IDE 1.16 ?
I have the NUCLEO-L552ZE-Q, and using the Cube programmer I can program the .elf to flash as it seems, which takes like 30 seconds.
When I debug from the Cube IDE 1.16 it takes very short time and I see no dowloading of my .elf.
How can I download my application automatically when going to debug.
2024-07-15 08:09 AM
It should do the download when you press the 'Debug' button, but you're not the first today saying that it doesn't:
2024-07-15 08:44 AM
Thanks Andrew,
It starts working w. 1.15.1.
-sten