cancel
Showing results for 
Search instead for 
Did you mean: 

debug CubeIDE

RFREN.1
Associate II

Hello,

I made a software on the STM32F469-Disco and now, I would like to use the same project on the STM32F479VI with the MB1166 (touch screen).

If I create a new project, no problem, I can flash the microcontroller.

If I start from the software made on the demoboard, I can compile but I cant' debut and I'have got the information in attachment.

So I can conclude that the problem is software. I think, with the picture that is a device issue.

What is your point of view.

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Imen.D
ST Employee

Hello @RFREN.1​ ,

Have you tried with different boards/MCUs ?

Try select "Erasing & Programming" on the left, then do a "Full chip erase".

If your issue is solved, please select the answe as “Best�? as this will help other users to find this response faster.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
RFREN.1
Associate II

Hello,

Thanks for your comments. A made a full erase and it's not working.

How Can I change MCU from an existing project ?

Thank you

Best Regards

RFREN.1
Associate II

If you want we can make a call to see together the issu and I will share my screen.

Imen.D
ST Employee

Try using SWD mode instead of JTAG, and check the assignment of the SWD pins.

Maybe your code into low-power modes.

Are you using "connect under reset" or "software system reset" mode?

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
RFREN.1
Associate II

Hello, I success to put the program the microcontroleur. thank for your help.

Now, I have another problem. The PLL for DSI doesn't to lock.

See the code generated automaticly by STM32CubeIDE.

No flag come to pass the "WHILE".