2024-12-20 01:46 AM - last edited on 2024-12-20 02:12 AM by mƎALLEm
hello i downdload latest version but again this error will come when i press migrate or continue option after that iam updating my code in this code goes to error part. fix this problem.
2024-12-20 03:32 AM
@syedhashmiraza wrote:
yes i tried this one but still code not working
Share again the screenshot with that option.
And again check if you have C:/Users/Ciright/STM32Cube/Repository/STM32Cube_FW_F4_V1.28.1on your local disk drive --> please confirm that
2024-12-20 04:31 AM - edited 2024-12-20 04:32 AM
iam facing same problem
2024-12-20 04:39 AM
After checking that option, did you regenerate the code and click on "Migrate"?
2024-12-20 05:36 AM
yes i did this but still error will come after i genrate code
2024-12-20 05:50 AM
@Ghofrane GSOURI could help you on that.
2024-12-20 06:44 AM
Hello @syedhashmiraza
Let's try this:
- Close the CubeMX.
- Go to C:\Users\XXXX and delete .stm32cubemx
- Then Reopen the CubeMX 6.13.0 load your IOC.
THX
Ghofrane
2024-12-21 05:28 AM
This is NOT an ERROR.
It is a SWITCH between 2 options.
In xx.ioc editor, project manager tab, check if "Use latest version" is checked.
If checked, every time you start edit an .ioc you can decide between 2 options, old version or new version
2024-12-24 10:20 PM - edited 2024-12-24 10:24 PM
hello,When i generate and migrate the code, my biometric code goes into the error part, but when I don't generate the code, my code runs properly. However, I need to integrate UART into it.
2024-12-24 10:21 PM
hello,When I integrate UART and generate and migrate the code, my biometric code goes into the error part, but when I don't generate the code, my code runs properly. However, I need to integrate UART into it
2024-12-25 12:15 AM
If the original question has been answered (posted in your first comment). Please accept as solution the comment that answered your question and open a new thread for the new request.
Thank you for your understanding.