cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMx error

syedhashmiraza
Associate II

hello i downdload latest version but again this error will come when i press migrate or continue option after that iam updating my code in this code  goes to  error part. fix this problem.

 

Screenshot 2024-12-20 133438.png

31 REPLIES 31
Ghofrane GSOURI
ST Employee

Hello @syedhashmiraza 

Could you please explain more about the error that you are facing?

THX

Ghofrane

mÆŽALLEm
ST Employee

Hello,

Check if V1.28.1 is available in this path: C:/Users/<user name>/STM32Cube/Repository/

SofLit_0-1734688668123.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

syedhashmiraza_0-1734690830478.png

 

I mean check that you have STM32Cube_FW_F4_V1.28.1 folder at this drive location: C:/Users/Ciright/STM32Cube/Repository/

SofLit_0-1734691443326.png

Otherwise, check the checkbox: "Use Default Firmware Location":

SofLit_1-1734691643081.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

syedhashmiraza_0-1734692398820.png

 

You shared the same screenshot here.

I've already suggested, either:

1- to check if you have  C:/Users/Ciright/STM32Cube/Repository/STM32Cube_FW_F4_V1.28.1 path on your drive.

or, check the checkbox: "Use Default Firmware Location" and regenerate the code. Normally CubeMx will download the missing package:

2- SofLit_1-1734691643081.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

i tried this one but still after i genarate code , shows error ?how can solve this error?

yes i tried this one but still code not working

But I don't see from your shared screenshot you checked the option:  "Use Default Firmware Location":

SofLit_1-1734691643081.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.