2024-03-13 10:08 AM
Hello,
when i click on a .ioc file within CubeIDE, CubeMX is opened inside of CubeIDE. It starts opening the ioc file and shows progress bars:
But then, after opening, it shows only a tab with no content.
Does someone know whats wrong here?
I use:
Debian Linux 11.9
CubeMX 6.10.0
CubeIDE 1.14.0
Thank you.
2024-03-14 05:16 AM
Hello @sk-st
First let me thank you for posting.
Could you provide .ide.log and the .log file from the workspace project.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-14 07:44 AM