cancel
Showing results for 
Search instead for 
Did you mean: 

Cubeide v1.19.0 - can't enable QSPI

MMARI.1
Senior

hi,

cube ide updated with latest version  1.19.0 have bug as below picture .

By default quad spi is disabled and i could able to select quad spi in older version cube mx by using old project and continue with old cube mx version not migrate .

MMARI1_0-1752666904539.png

 

3 REPLIES 3
Andrew Neil
Super User

you haven't said what chip you're using!

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

hi neil,

stm32h723zgt6 with w25q128

Mahmoud Ben Romdhane
ST Employee

Hello @MMARI.1 ,

 

The same issue was reported on these posts:

STM32CubeIDE 1.19.0 Problem migrating OCTOSPI2 (ST... - STMicroelectronics Community

STM32CUBEIDE Version: 1.19.0 QUADSPI unavailable ... - STMicroelectronics Community

An Internal Ticket was raised to the Development Team ( Ticket Number: 213718 ).

 

Thanks.

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.