cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE opens random files on debug start / end

CBerg
Senior

Since a while - I guess since update 1.8 or something - CubeIDE opens random project *.c-files, when the debug process is started or stopped.

In this example only main.c was open. When I clicked on "debug", "startup_stm32_g473vetx.s" was openend, and when I stopped the debug session, "stm32g4xx_hal_spi.c" was opened.

a.png

This is pretty annoying, because you have to close them manually or your edit window will fill up with open files, you do not want to have open.

Please fix that.

2 REPLIES 2
TDK
Guru

This has to be the most annoying and time wasting bug in CubeIDE. @mattias norlander any updates?

See explanation here:

https://community.st.com/t5/stm32-mcus-touch-gfx-and-gui/how-to-stop-stm32cubeide-from-opening-random-files-when-debug-is/td-p/98917

If you feel a post has answered your question, please click "Accept as Solution".
padawan
Senior

Hi 

https://wiki.st.com/stm32mcu/wiki/STM32CubeIDE:STM32CubeIDE_errata_1.13.x says that the issue ID 139768 is solved. 

But this is lie. They may testet it at the first run, but not at a seconde one.

padawan