cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE not loading source code for makefile project while debugging

gkowshik
Associate II

Hi All,

I have a Makefile based project that I imported to CubeIDE. I am able to build it smooth, however when i am trying to launch a debug window I am not able to see the source code and it only shows 2 buttons saying "View Disassembly" and Preferences tab.

Unlike the one's shown online I am not getting an option to load the source file by browsing my file system. What am I doing wrong and how to load this??

The below is my debugger view (I put a breakpoint at Reset_Handler hence the halt)

gkowshik_0-1727861635969.png

 

Please help me with the problem as it's very hard to debug with the assembly view. please note the view is not loading when the function is entering C files too, i.e., from Reset Handler the PC jumps to SystemInit which here is a C file but even for that I am not able to see the load.

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions

@gkowshik wrote:

Did you build with debug info? - Do you mean my optimization level? Yes, I had -O0 and added 


No. You need a -g to include debug info in the ELF file:

https://gcc.gnu.org/onlinedocs/gcc/Debugging-Options.html#:~:text=Level%203%20includes%20extra%20information%2C%20such%20as%20all%20the%20macro%20definitions%20present%20in%20the%20program 

 

Default for CubeIDE is -g3:

AndrewNeil_0-1727865097015.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

View solution in original post

6 REPLIES 6
Andrew Neil
Super User

What version of GCC do you use to build?

Did you build with debug info?

What version of CubeIDE do you use to debug?

 


@gkowshik wrote:

when i am trying to launch a debug window I am not able to see the source code


Show how you do the launch

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
gkowshik
Associate II

What version of GCC do you use to build? - gcc version 10.3.1 20210621 (release) (15:10.3-2021.07-4)

Did you build with debug info? - Do you mean my optimization level? Yes, I had -O0 and added 

What version of CubeIDE do you use to debug? - I am using the latest version i.e., 1.16.1

Show how you do the launch

I created a new debug configuration by going to Run -> Debug Configurations

gkowshik_0-1727864353421.png

gkowshik_1-1727864373445.png

gkowshik_2-1727864386443.png

 

And to launch I simply clicked Debug As -> STM32 C/C++ Application and it was able to launch it.

 

 


@gkowshik wrote:

Did you build with debug info? - Do you mean my optimization level? Yes, I had -O0 and added 


No. You need a -g to include debug info in the ELF file:

https://gcc.gnu.org/onlinedocs/gcc/Debugging-Options.html#:~:text=Level%203%20includes%20extra%20information%2C%20such%20as%20all%20the%20macro%20definitions%20present%20in%20the%20program 

 

Default for CubeIDE is -g3:

AndrewNeil_0-1727865097015.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi,

Thanks for pointing it out. I have now included it in my makefile. Here's my makefile for your reference, however I am still not being able to reference the source code while loading the elf in the IDE.

 

 

TARGET=main EXECUTABLE=main.elf BINARYOUT=main.bin MAPFILE=main.map # Define the map file name # STLINK=~/Downloads/stlink LIBPATH=STM32L1xx_StdPeriph_Lib/ CC=arm-none-eabi-gcc LD=arm-none-eabi-gcc AR=arm-none-eabi-ar AS=arm-none-eabi-as CP=arm-none-eabi-objcopy OD=arm-none-eabi-objdump BIN=$(CP) -O ihex DEFS = -DUSE_STDPERIPH_DRIVER -DSTM32L1XX -DHSE_VALUE=8000000 -DSTM32L1XX_MD STARTUP = $(LIBPATH)/Libraries/CMSIS/Device/ST/STM32L1xx/Source/Templates/gcc_ride7/startup_stm32l1xx_md.s MCU = cortex-m3 MCFLAGS = -mcpu=$(MCU) -mthumb -mlittle-endian -mfloat-abi=soft -std=gnu11 -g3 ASMFLAGS = -mcpu=$(MCU) -mthumb -mlittle-endian -mfloat-abi=soft -g3 STM32_INCLUDES = -I$(LIBPATH)/Libraries/CMSIS/Device/ST/STM32L1xx/Include/ \ -I$(LIBPATH)/Libraries/CMSIS/Include/ \ -I$(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/inc/ \ -I./inc/ \ -I./inc/BLE/ OPTIMIZE = -O0 # Separate CFLAGS (for compilation) and LDFLAGS (for linking) CFLAGS = $(MCFLAGS) $(OPTIMIZE) $(DEFS) -I. -I./ $(STM32_INCLUDES) LDFLAGS = -Wl,-T,stm32_flash.ld -Wl,-Map=$(MAPFILE) src=./src/main.c \ ./src/millis.c \ ./src/usart.c \ ./src/spi.c \ ./src/debug.c \ ./src/stm32l1xx_it.c \ ./src/system_stm32l1xx.c \ ./src/BLE/io_support.c \ ./src/BLE/acilib.c \ ./src/BLE/aci_queue.c \ ./src/BLE/aci_setup.c \ ./src/BLE/hal_aci_tl.c \ ./src/BLE/lib_aci.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_gpio.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_spi.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/misc.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_dbgmcu.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_dma.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_exti.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_flash.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_i2c.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_iwdg.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_pwr.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_rcc.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_rtc.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_sdio.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_syscfg.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_tim.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_usart.c \ $(LIBPATH)/Libraries/STM32L1xx_StdPeriph_Driver/src/stm32l1xx_wwdg.c # Object files OBJDIR = . OBJ = $(SRC:%.c=$(OBJDIR)/%.o) STARTUP_OBJ = $(STARTUP:%.s=$(OBJDIR)/%.o) all: $(TARGET) $(TARGET): $(EXECUTABLE) $(CP) -O ihex $(EXECUTABLE) $(TARGET).hex $(CP) -O binary $(EXECUTABLE) $(BINARYOUT) $(EXECUTABLE): $(OBJ) $(STARTUP_OBJ) $(CC) $(CFLAGS) $(OBJ) $(STARTUP_OBJ) $(LDFLAGS) -lm -lc -lnosys -o $(EXECUTABLE) $(OBJDIR)/%.o: %.c $(CC) $(CFLAGS) -c $< -o $@ $(OBJDIR)/%.o: %.s $(AS) $(ASMFLAGS) -c $< -o $@ clean: rm -f $(OBJDIR)/src/*.o \ $(OBJDIR)/src/BLE/*.o \ $(OBJDIR)/STM32L1xx_StdPeriph_Lib/Libraries/STM32L1xx_StdPeriph_Driver/src/*.o \ $(TARGET) \ $(EXECUTABLE) \ $(BINARYOUT) \ $(TARGET).hex \ $(MAPFILE) # Remove the map file
View more

 

I have somehow solved this issue by selecting the MCU name in the Build settings, then when I put a breakpoint to a function that's in a C file, it didn't load the source code directly however it has now brought the button to search and load the source file.

gkowshik_0-1727866746133.png

 

gkowshik
Associate II

@elif77 Thanks for the reply. There seems to be a mismatch in the cross referencing of the file path as my PC has WSL enabled and I need to add the mapping translations for the file path in the debug configuration. 

After giving the file paths and the mainly enabling "-g3" to the makefile I am able to get the debug views correctly. 

Thanks alot for your help, I will close this.

gkowshik_0-1727874201073.png