cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE / MX Download Issue

Maximilian Pohl
Associate III

Hello, 

i just installed CubeIDE / MX on a brand new Computer. I am running Windows 11.

Both IDE and MX have a problem with downloading "software packages" The are extremly slow and after an hour i get an error message. I am not able to work with that behaviour. 

I checked the Firewall / Disabled it. Internet connection is there, and yes it is fast enough. All other programs works just fine.

Its just the ST Tools. 

Is there any known issue with windows 11?

Hope someone can help me, because i would like to continue with my projects.

 

Best regards

Max

3 REPLIES 3
SabTuna
Associate II

can you specify the error message? 

MaximilianPohl_0-1733919102528.png

 

Hello,

I think the cube package F4 V1.18.1 is no more available for download from ST website.

The oldest version available is at this date is V1.23.0.

SofLit_0-1733932737982.png

So either you configure your project to point to the latest version of the HAL or open an ols ticket to get F4 V1.18.1.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.