2020-01-21 09:14 AM
CubeIDE 1.21 causes 100% processor usage and slows down the computer. Even worse is closing the program doesn't free up the resources, the usage still stays 100%. The task manager shows that cubeide.exe closes, but still the issue stays. I'm running windows 7 pro x64.
2020-01-27 10:03 PM
just remove and againg install,
otherwise problem may be in your pc
2020-01-27 10:03 PM
mostly it depends on ram
2020-01-27 10:15 PM
My computer has 16GB of ram, task manager shows about 10GB in use, so that shouldn't be an issue. I have also a laptop where it runs normally (windows 10). BTW, Cubeide 1.1 run normally. Problems started when started using 1.2.
2020-01-27 10:30 PM
Other Eclipse-nased tools use to run for a couple of seconds after closing as well, so this is nothing special.
After a minute at latest, it should be gone.
Check the ressource usage at runtime, before and during operation. Including HD throughput.
And I would try with the network cable pulled out.
2020-01-28 02:44 AM
just submit a ticket to silabs