CubeIDE 1.18 cannot detect ST-Link anymore
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-18 7:38 AM - edited ‎2025-03-18 8:20 AM
Hi,
starting with Update 1.18 (update from 1.17) sth. broke and i cannot debug anymore.
I tried a nucleo Board with integrated St-Link and an ST-Link V3. All Screenshots were done with the v3 St-Link
I reinstalled CubeIDE already from the complete download-package, but still the same problem
i always get
But the update works ( so my st-link is found)
I can flash my image via st-link utility without problems.
but cannot get debug to work with 1.18.
With v1.17 i had no problems at all and debugging worked flawlessly.
So what can i do to fix this?
i tried with stlink-v3 and v2.1
and i use Windows 11 Enterprise
Regards
Solved! Go to Solution.
- Labels:
-
STM32CubeIDE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-24 2:46 AM
@funky wrote:ok, i'm starting to cry. monday morning in the office. same problem again.
So have you re-checked the firewall settings?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-24 5:33 AM - edited ‎2025-03-24 5:35 AM
yes, checked settings again, looking fine
current state:
i reboot and my stm32cubeprogrammer looks like this:
as soon as i click sth the connection to st-link is lost is lost
CubeIDE with gdb autostart...no st-link detected message box
CubeIDE, switch debugger to "connect to remote gdb" and start my gbd via commandline and it works
C:\ST\STM32CubeIDE_1.18.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_2.2.100.202501151542\tools\bin\ST-LINK_gdbserver.exe -p 61634 -l 1 -d -z 61265 -i 004000283133510736303739 -cp C:\ST\STM32CubeIDE_1.18.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.100.202412061334\tools\bin -m 0 -g --frequency 24000
STMicroelectronics ST-LINK GDB server. Version 7.10.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61634
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.19.0
-------------------------------------------------------------------
Log output file: C:\###\STM32CubeProgrammer_a22220.log
ST-LINK SN : 004000283133510736303739
ST-LINK FW : V3J15M7B5S1
Board : STLINK-V3SET
Voltage : 3.27V
SWD freq : 8000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x413
Revision ID : Rev Y
Device name : STM32F405xx/F407xx/F415xx/F417xx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0x31
Opening and parsing file: ST-LINK_GDB_server_a22220.srec
Memory Programming ...
File : ST-LINK_GDB_server_a22220.srec
Size : 621.88 KB
Address : 0x08000000
Erasing memory corresponding to sector 0:
Erasing internal memory sectors [0 1]
Erasing memory corresponding to sector 0:
Erasing internal memory sectors [5 9]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:10.625
at least i can debug somehow but it is not nice but i don't know what causes this and wasted days for this :(

- « Previous
- Next »