CubeIDE 1.18 cannot detect ST-Link anymore
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-18 7:38 AM - edited ‎2025-03-18 8:20 AM
Hi,
starting with Update 1.18 (update from 1.17) sth. broke and i cannot debug anymore.
I tried a nucleo Board with integrated St-Link and an ST-Link V3. All Screenshots were done with the v3 St-Link
I reinstalled CubeIDE already from the complete download-package, but still the same problem
i always get
But the update works ( so my st-link is found)
I can flash my image via st-link utility without problems.
but cannot get debug to work with 1.18.
With v1.17 i had no problems at all and debugging worked flawlessly.
So what can i do to fix this?
i tried with stlink-v3 and v2.1
and i use Windows 11 Enterprise
Regards
Solved! Go to Solution.
- Labels:
-
STM32CubeIDE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-21 7:03 AM
nope, nothing.
And as said...in the debugging configuration the IDE detects my st-link. But it is not usable when i want to debug.
I'm out of ideas
I downgraded the IDE, uninstalled all (old) drivers/devices in the device manager, nothing helps
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-21 7:18 AM
Show the console log from when CubeIDE tries to start a debug session.
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-21 9:06 AM - edited ‎2025-03-24 12:43 AM
the firewall was the problem. i deleted all cubeide entries in the firewall and when i started the IDE there was a firewall message that gdb server wants to connect. i just accepted that. same problem...no connection
now i deleted the entries in the firewall and checked again. in the defaults there weren't all networks selected/allowed. i selected everything and accepted and suddenly my gdb server is started again and i can debug.
now i also see my st-link in the programmer again
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-21 9:34 AM
good !
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-21 9:44 AM
So same issue as here: https://community.st.com/t5/stm32cubeide-mcus/st-link-error-failed-to-bind-to-port-61235-failure-starting-swv/m-p/784642 ?
Did you not get any error messages like that one?
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-24 12:42 AM
No, the whole gdb-server start output was missing
I did not see the whole startup output. As soon as i pressed the debug button the message box with the missing st-link notice appeared and none of the gdb server output
i don't know what triggered my firewall to behave like this. Because i'm pretty sure when i first installed cubeIDE in the past i did not hit any extra checkboxes in the firewall configuration.
And my colleagues who also use cubeIDE 1.18 did not have these problems and everything worked flawlessly after the update
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-24 1:22 AM
ok, i'm starting to cry. monday morning in the office. same problem again.
no st-link found, no gdbserver started. (on friday i was at home so little different network setup)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-24 1:46 AM
ok... it seems the autostart of the gdb server does not work anymore. i absolutley do not know why.
in the debugger configuration there is the "show command line" button for the gdb server start. if i copy that command and start it manually via commandline i get another firewall popup for my gdb server, i accept that and my gdb server is started and listening for connection. when i configure my settings to connect to a remote gdb server with that port everthing works fine i can start my program and debug.
when i switch back to autostart local gdb server, nothing is started i get the no st-link connected message instantly
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-24 2:01 AM - edited ‎2025-03-24 2:04 AM
after starting that gdb server manually it worked one time and now i switched back to automatic start and i get after reboot this logoutput ONCE
STMicroelectronics ST-LINK GDB server. Version 7.10.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name :...\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 6124
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
ST-Link enumeration failed
Error in initializing ST-LINK device.
Reason: ST-LINK DLL error.
and the next try the "NO ST-Link detected" message box is back again.
this is *^°?!#111 :D
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-24 2:25 AM
Hi,
so : >
Reason: ST-LINK DLL error.
Just try:
close IDE ;
load/install (actual) STM32CubeProgrammer , check connection to board (maybe : update st-link);
then try IDE again.