cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE 1.18 cannot detect ST-Link anymore

funky
Associate III

Hi,

starting with Update 1.18  (update from 1.17) sth. broke and i cannot debug anymore.
I tried a nucleo Board with integrated St-Link and an ST-Link V3. All Screenshots were done with the v3 St-Link
I reinstalled CubeIDE already from the complete download-package, but still the same problem

i always get
funky_0-1742308417257.png

But the update works ( so my st-link is found)

funky_1-1742308536498.png

funky_2-1742308587232.png

I can flash my image via st-link utility without problems.

but cannot get debug to work with 1.18.

With v1.17 i had no problems at all and debugging worked flawlessly.

So what can i do to fix this?

i tried with stlink-v3 and v2.1

and i use Windows 11 Enterprise
Regards

4 REPLIES 4

@funky wrote:

I can flash my image via st-link utility without problems.


What about CubeProgrammer?

did not use it until now but will check

funky
Associate III

hmmm...interesting. cubeprogrammer does not detect my st-link?!

funky
Associate III

funky_0-1742310342731.png

this is what my device manager shows me. it is an st-link v3 but with the nucleo st-link v2 it is also not working :(

in the cubeprogrammer: when i try to upgrade my st-link it wants to downgrade the firmware.
this is the version i get via cubeprogrammer

funky_1-1742310537744.png

and via stm32cubeide
funky_2-1742310618011.png