2024-05-25 12:59 PM
Hi,
It's freshly installed cubeide precisely. Version: 1.15.1 i created a project on stm32u545ret6q mcu. When i set up cubemx just for simple test/generate of code a small window pops up for a fraction of a second, and code is not generated.
This window has written "Progress Information".
I also see one warning: Project "InzStm" has no explicit encoding set.
2024-06-03 06:20 AM
Hello @gurdzinskidawid
First let me thank you for posting.
I made the test with the attached ioc and I was able to generate code.
Could you please share the STM32CubeMX.log file found under /user/.stm32cubemx folder.
Or run CubeMX with the command line and share the content of the console.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.