2024-04-16 07:35 PM
I just re installed windows 10 and re installed the cube ide. Then when I try to create a project it crashes
I attached the log file for anyone who may can find why
2024-04-29 01:24 PM
Hello @crab,
Make sure it is not a known issue listed in this page STM32CubeIDE errata 1.15.x.
(like: having some spaces in the paths or installation path is not supported)