2023-06-22 8:13 AM
I am encountering an issue where a hard fault occurs when the "char * pszCommand" variable is written to because it is trying to change data that is not in the RAM.
Here is the related code that gives me the hard fault:
typedef struct
{
char * pszCommand; // command string
void (* pfnHandler)(Parsed_t * ParsedCmd); // handler function
int iParent; // index of command one level up in tree (if any)
int nRequiredLength; // number of significant chars in command
int nTreeLevel; // this commands depth in menu tree
unsigned short bBranchEnd:1; // set if this command is the end of branch
unsigned short bQueryAllowed: 1; // set if this command accepts queries
} CmdTreeEntry_t;
CmdTreeEntry_t * pTreeEntry;
// initialize the root entry
pTreeEntry = &g_CmdTree[0];
*pTreeEntry->pszCommand = ITEM_SEPARATOR; <------ The hard fault occurs after execution of this line
pTreeEntry->iParent = -1;
pTreeEntry->nRequiredLength = 1;
pTreeEntry->nTreeLevel = 1;
pTreeEntry->bBranchEnd = FALSE;
pTreeEntry->bQueryAllowed = FALSE;
CmdTreeEntry_t g_CmdTree[] =
{
/* command string, handler */
{ " ", NULL }, /* MUST BE FIRST ENTRY IN TABLE ! */
{ ":*CAL??", calibration_query},
{ ":*CLS", clear_status_cmd},
.... (A bunch of commands)
{ NULL, NULL} /* MUST BE LAST ENTRY IN TABLE!!! */
};
I believe this is somehow related to the linker file not allocating the memory properly for the pszCommand pointer, but I am unable to find where the issue may be in the linker.
Here is the linker file:
/* Entry Point */
ENTRY(Reset_Handler)
/* Highest address of the user mode stack */
_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */
_Min_Heap_Size = 0x200; /* required amount of heap */
_Min_Stack_Size = 0x400; /* required amount of stack */
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 512K
}
/* Sections */
SECTIONS
{
/* The startup code into "FLASH" Rom type memory */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH
/* The program code and other data into "FLASH" Rom type memory */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
_etext = .; /* define a global symbols at end of code */
} >FLASH
/* Constant data into "FLASH" Rom type memory */
.rodata :
{
. = ALIGN(4);
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
. = ALIGN(4);
} >FLASH
.ARM.extab : {
. = ALIGN(4);
*(.ARM.extab* .gnu.linkonce.armextab.*)
. = ALIGN(4);
} >FLASH
.ARM : {
. = ALIGN(4);
__exidx_start = .;
*(.ARM.exidx*)
__exidx_end = .;
. = ALIGN(4);
} >FLASH
.preinit_array :
{
. = ALIGN(4);
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP (*(.preinit_array*))
PROVIDE_HIDDEN (__preinit_array_end = .);
. = ALIGN(4);
} >FLASH
.init_array :
{
. = ALIGN(4);
PROVIDE_HIDDEN (__init_array_start = .);
KEEP (*(SORT(.init_array.*)))
KEEP (*(.init_array*))
PROVIDE_HIDDEN (__init_array_end = .);
. = ALIGN(4);
} >FLASH
.fini_array :
{
. = ALIGN(4);
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
. = ALIGN(4);
} >FLASH
/* Used by the startup to initialize data */
_sidata = LOADADDR(.data);
/* Initialized data sections into "RAM" Ram type memory */
.data :
{
. = ALIGN(4);
_sdata = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
*(.RamFunc) /* .RamFunc sections */
*(.RamFunc*) /* .RamFunc* sections */
. = ALIGN(4);
_edata = .; /* define a global symbol at data end */
} >RAM AT> FLASH
/* Uninitialized data section into "RAM" Ram type memory */
. = ALIGN(4);
.bss :
{
/* This is used by the startup in order to initialize the .bss section */
_sbss = .; /* define a global symbol at bss start */
__bss_start__ = _sbss;
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
_ebss = .; /* define a global symbol at bss end */
__bss_end__ = _ebss;
} >RAM
/* User_heap_stack section, used to check that there is enough "RAM" Ram type memory left */
._user_heap_stack :
{
. = ALIGN(8);
PROVIDE ( end = . );
PROVIDE ( _end = . );
. = . + _Min_Heap_Size;
. = . + _Min_Stack_Size;
. = ALIGN(8);
} >RAM
/* Remove information from the compiler libraries */
/DISCARD/ :
{
libc.a ( * )
libm.a ( * )
libgcc.a ( * )
}
.ARM.attributes 0 : { *(.ARM.attributes) }
}
This is the memory address of pTreeEntry that is being placed in RAM but the address of pszCommand is not in RAM.
Any help would be appreciated.
Thanks,
Dan
Solved! Go to Solution.
2023-06-27 12:37 PM
I found a solution that works, thanks to a coworker of mine that had some helpful insight. I created a new function that will allocate RAM space for the character and copy it from ROM.
static char * ROMtoRAM(char pszCommandContents[]){
size_t len = strlen(pszCommandContents) + 1;
char * target = malloc(len);
if (target == NULL) return NULL;
memcpy(target, pszCommandContents, len);
return target;
}
With this function I can change where pTreeEntry->pszCommand is being pointed to and can actually write to the allocated memory.
pTreeEntry->pszCommand = ROMtoRAM(pTreeEntry->pszCommand);
*pTreeEntry->pszCommand = ITEM_SEPARATOR;
I think this is acceptable to use so that it doesn't hard fault.
2023-06-22 9:03 AM
The line
*pTreeEntry->pszCommand = ITEM_SEPARATOR;
should give you at least a warning, which you should not ignore. The * in front is wrong. Note that string literals are
purposely stored in Flash, not RAM.
hth
KnarfB
2023-06-22 9:44 AM
For some reason, the inverse gives me a warning. There is no warning when it compiles with the * in front but when I remove it I get this warning:
2023-06-22 9:54 AM
If I run it without the * in front of pTreeEntry the variable gets the correct value as well as a bunch of other repeating stuff.
However, the next time pTreeEntry->pszCommand is written to I get a hard fault again.
// remove leading ':' chars from string
if( iChar )
strcpy( pTreeEntry->pszCommand, pTreeEntry->pszCommand + iChar );
2023-06-22 10:20 AM - edited 2023-06-22 10:22 AM
Please debug your program; try to understand why *pTreeEntry->pszCommand does not point to RAM.
If you have not used the debugger yet, this is a perfect opportunity to get know the debugger.
By the way, more clear (less confusing) syntax would be:
pTreeEntry->pszCommand[0] = ITEM_SEPARATOR;
2023-06-22 12:20 PM
I have been using the debugger but without any success. I do not understand why it is pointing to ROM and not RAM, because the g_CmdTree has the pszCommand initialized in RAM but when pTreeEntry is set to the address of g_CmdTree[0] it is only seeing the ROM address.
2023-06-22 12:37 PM
Ok so you are already on the right way. Solving issues like this may be a exciting experience, take your time and enjoy.
2023-06-22 1:03 PM
We don't see your definition of ITEM_SEPARATOR, but the name pszCommand suggests, it should be a string like "XYZ". Then,
is valid, but
is not (warning: assignment to 'char' from 'char *' makes integer from pointer without a cast).
Keep in mind, that pszCommand is only a pointer, pointing to some memory/string, but not an array containing a string. So the strcpy below is dangerous and may fail if the string pszCommand points to is in the Flash.
hth
KnarfB
2023-06-22 1:30 PM
Here is the definition of ITEM_SEPARATOR:
// separator between items in a command
#define ITEM_SEPARATOR ':'
I see what you are saying now about the * in front of pTreeEntry when I replace ITEM_SEPARATOR with ":" I get the same warning.
Do you know a better way to accomplish the strcpy that is being attempted here? Sorry I am not super well versed in C and this code was written by someone around 25-30 years ago.
2023-06-22 2:33 PM
Use
#define ITEM_SEPARATOR ":" // USE STRING NOT CHAR BRACING
pTreeEntry->pszCommand = ITEM_SEPARATOR; // CHANGE THE POINTER TO THE NEW STRING
pTreeEntry and the pointer are in RAM, they can POINT to something in FLASH which is static.
pTreeEntry->pszCommand = strmalloc(newstring);