cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot install STM32 CubeIDE

YangHu
Associate

Hello,

I click the https://www.st.com/en/development-tools/stm32cubeide.html  link to download STM32 Cube IDE,and file name is "en.st-stm32cubeide_1.17.0_23558_20241125_2245_x86_64.exe.zip", MD5 is "157232C6532A28921F12A5E2A368253B".

 

But when i unzip this file, the 7zip note that End-of-file error.

I removed the.zip suffix manually and now the file suffix is.exe. windows says that the application cannot be installed.

 

Please help me install this software correctly.

- windows 10, x64

- RAM is 32G

 

BR,

Yang

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

It could be your download is not complete and you should not modify the file extension to exe. It's basically .exe compressed in zip format. So check you internet connection.

What is the size of the downloaded zip file? Its should be 1 090 862 kB

MD5: 2341c83a14f80feb7dc9d969d6550faf

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

Hello,

It could be your download is not complete and you should not modify the file extension to exe. It's basically .exe compressed in zip format. So check you internet connection.

What is the size of the downloaded zip file? Its should be 1 090 862 kB

MD5: 2341c83a14f80feb7dc9d969d6550faf

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.