cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot download project to target but IDE inform completed

_binhvo1003
Associate

Hi, 

I have an issue with my Nucleo-F446RE. There is a big project from my client, I already download it to target and it runs perfectly fine. But on tomorrow, when I perform a download of my Test project to the target, then I re-download the project of my client. The IDE still not appear any error and inform download complete but the target cannot get the download anymore, there is still my Test project in the board. But the strange thing is, I try to download another project and it still fine, so just my client's project has problem. But it is still can download before.

So do anyone meet this situation before? Please help!!

1 REPLY 1
mƎALLEm
ST Employee

Hello @_binhvo1003 and welcome to the community,

Sorry, this statement is not clear:


@_binhvo1003 wrote:

The IDE still not appear any error and inform download complete but the target cannot get the download anymore, there is still my Test project in the board.


The customer application CubeIDE upload is OK but the application doesn't run? 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.