2020-07-31 10:33 AM
I had some trouble to install STM32Cube 1.4.0 and I did a deinstallation via Windows Apps-Tool.
Also I delete some Registrieentries.
Now I can't Install STM32Cube 1.4.0 via
st-stm32cubeide_1.4.0_7511_20200720_0928_x86_64.exe
When I start the exe I get
I guess there is a "secret" entry that prevents the Installation.
How can I delete this entry?
Or what else can I do?
Best regards
Georg Münch
2020-08-01 1:51 PM
> Also I delete some Registrieentries.
This is bad. After tampering with the registry, all bets are off. Try System Restore.
--pa