cancel
Showing results for 
Search instead for 
Did you mean: 

Can't flash STM32H735IG discovery kit using S32CubeIDE

Elimathew72
Associate II

Hello all,

We are trying to evaluate the STM32H735IG for our product. We bought the off-the-shelf dev kit and tried flashing it using S32CubeIDE, but encountered an error. The weird thing is, I can use S32 programmer to read flash, so the ST-Link seems to be up-to-date. I feel there is something wrong with S32CubeIDE. Can you please help.

All the versions are below and also some screenshots to assist help debugging

STM32CubeIDE


Version: 1.14.0
Build: 19471_20231121_1200 (UTC)
OS: Linux, v.6.5.0-27-generic, x86_64 / gtk 3.24.33
Java vendor: Eclipse Adoptium
Java runtime version: 17.0.8.1+1
Java version: 17.0.8.1

Logs in the error window

Error in final launch sequence:

Failed to execute MI command:
load /home/STM32CubeIDE/workspace_1.14.0/BSP/STM32CubeIDE/Debug/BSP.elf

Error message from debugger back end:
Load failed
Failed to execute MI command:
load /home/STM32CubeIDE/workspace_1.14.0/BSP/STM32CubeIDE/Debug/BSP.elf

Error message from debugger back end:
Load failed
Failed to execute MI command:
load /home/STM32CubeIDE/workspace_1.14.0/BSP/STM32CubeIDE/Debug/BSP.elf

Error message from debugger back end:
Load failed
Load failed

 

Logs in the console 

 

STMicroelectronics ST-LINK GDB server. Version 7.5.0

Copyright (c) 2023, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

 

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Shutting down...

Exit.

 

 

 

10 REPLIES 10

Also tried it on MAC OS still the same any opinions @Rim LANDOLSI  , I saw your post https://community.st.com/t5/stm32cubeide-mcus/why-does-elf-load-fails-when-using-stm32cubeide/td-p/77016 

I see the gdbserver has the same error, also I am not modifying anything from the sample BSP example which comes out of the box.

[2.277] write(): <11> Tx: $E31#a9
[2.277] read(): <11> Rx: $vKill;a410#33
[2.277] handlePacket(): Hidden/Unsupported v-command 'vKill', see RSP for details
[2.277] write(): <11> Tx: $#00
[2.278] read(): <11> Rx: $k#6b