2024-05-21 09:04 PM
Hello all,
We are trying to evaluate the STM32H735IG for our product. We bought the off-the-shelf dev kit and tried flashing it using S32CubeIDE, but encountered an error. The weird thing is, I can use S32 programmer to read flash, so the ST-Link seems to be up-to-date. I feel there is something wrong with S32CubeIDE. Can you please help.
All the versions are below and also some screenshots to assist help debugging
STM32CubeIDE
Version: 1.14.0
Build: 19471_20231121_1200 (UTC)
OS: Linux, v.6.5.0-27-generic, x86_64 / gtk 3.24.33
Java vendor: Eclipse Adoptium
Java runtime version: 17.0.8.1+1
Java version: 17.0.8.1
Logs in the error window
Error in final launch sequence:
Failed to execute MI command:
load /home/STM32CubeIDE/workspace_1.14.0/BSP/STM32CubeIDE/Debug/BSP.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load /home/STM32CubeIDE/workspace_1.14.0/BSP/STM32CubeIDE/Debug/BSP.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load /home/STM32CubeIDE/workspace_1.14.0/BSP/STM32CubeIDE/Debug/BSP.elf
Error message from debugger back end:
Load failed
Load failed
Logs in the console
STMicroelectronics ST-LINK GDB server. Version 7.5.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Shutting down...
Exit.
2024-05-27 03:06 PM
Also tried it on MAC OS still the same any opinions @Rim LANDOLSI , I saw your post https://community.st.com/t5/stm32cubeide-mcus/why-does-elf-load-fails-when-using-stm32cubeide/td-p/77016
I see the gdbserver has the same error, also I am not modifying anything from the sample BSP example which comes out of the box.
[2.277] write(): <11> Tx: $E31#a9
[2.277] read(): <11> Rx: $vKill;a410#33
[2.277] handlePacket(): Hidden/Unsupported v-command 'vKill', see RSP for details
[2.277] write(): <11> Tx: $#00
[2.278] read(): <11> Rx: $k#6b