2024-07-09 07:24 AM
Hello,
I recently bought a NUCLEO-F412ZG and shortly downloaded STM32CubeIDE.
However, I only tried to debug and launch the generated program, without changing anything, and came across this error message :
Checked the path, all is good. I can't seem to compile any project.
Here are the logs from st-link_gdbserver_log.txt :
[0.000] initConfigParams(): Configuration flags start
[0.000] initConfigParams(): external-init false
[0.000] initConfigParams(): pend-halt-timeout (null)
[0.000] initConfigParams(): halt false
[0.000] initConfigParams(): config-file ""
[0.000] initConfigParams(): persistent false
[0.000] initConfigParams(): +log-file "C:\Users\xxx\Documents\STM32\First\Debug\st-link_gdbserver_log.txt"
[0.000] initConfigParams(): +log-level 31
[0.009] initConfigParams(): +port-number 61234
[0.009] initConfigParams(): +verbose true
[0.009] initConfigParams(): refresh-delay 15
[0.009] initConfigParams(): +verify true
[0.009] initConfigParams(): +swd true
[0.009] initConfigParams(): swo-port 61234
[0.009] initConfigParams(): cpu-clock 8000000
[0.009] initConfigParams(): swo-clock-div 128
[0.009] initConfigParams(): +initialize-reset true
[0.009] initConfigParams(): debuggers false
[0.009] initConfigParams(): serial-number ""
[0.009] initConfigParams(): +apid 0
[0.009] initConfigParams(): attach false
[0.009] initConfigParams(): shared false
[0.009] initConfigParams(): erase-all false
[0.009] initConfigParams(): memory-map ""
[0.009] initConfigParams(): ext-memory-loaders false
[0.009] initConfigParams(): extload_init (null)
[0.009] initConfigParams(): extload (null)
[0.009] initConfigParams(): +stm32cubeprogrammer-path "C:\ST\STM32CubeIDE_1.15.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.201.202404072231\tools\bin"
[0.009] initConfigParams(): temp-path ""
[0.009] initConfigParams(): preserve-temps false
[0.009] initConfigParams(): frequency 0
[0.009] initConfigParams(): licenses false
[0.009] initConfigParams(): ignore-rest false
[0.009] initConfigParams(): version false
[0.009] initConfigParams(): help false
[0.009] initConfigParams(): Configuration flags end
[0.010] init(): STMicroelectronics ST-LINK GDB server. Version 7.7.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
[0.077] openDevice(): COM frequency = 4000 kHz
[0.077] openDevice(): Target connection mode: Under reset
[0.085] readFromTarget(): Reading ROM table for AP 0 @0xe00fffd0
[0.088] reset_hw_wtchpt_module(): Hardware watchpoint supported by the target
[0.091] initContext(): ST-LINK Firmware version : V2J45M30
[0.092] initContext(): Device ID: 0x441
[0.092] initContext(): PC: 0x800893c
[0.092] Device_GetStatus(): ST-LINK device status: HALT_MODE
[0.092] initContext(): ST-LINK detects target voltage = 3.24 V
[0.093] initContext(): ST-LINK device status: HALT_MODE
[0.093] initServerContext(): ST-LINK device initialization OK
[0.093] pollAndNotifyRun(): Stm32Device, pollAndNotify running...
[0.095] updateState(): SwvSrv state change: 0 -> 1
[0.095] WaitConnection(): Waiting for connection on port 61234...
[0.095] WaitConnection(): Waiting for connection on port 61235...
[2.142] stop(): Stopping port 61234
[2.172] WaitConnection(): Received stop for port 61234, not accepting new connections.
[2.172] deInit(): GdbSrv, deInit entry.
[2.172] deInit(): GdbSessionManager, deInit entry.
[2.282] deInit(): GdbSessionManager, deInit exit
[2.282] deInit(): SwvSrv deInit entry
[2.282] stop(): Stopping port 61235
[2.391] WaitConnection(): Received stop for port 61235, not accepting new connections.
[2.391] deInit(): SwvSrv deInit exit
[2.391] closeDevice(): Stm32Device, closeDevice() entry
[2.502] pollAndNotifyRun(): Stm32Device, pollAndNotify stopped
[2.507] closeDevice(): Stm32Device, closeDevice() exit
[2.507] deInit(): Stm32Device, deInit success
[2.507] deInit(): GdbSrv, deInit exit.
I tried other ports and rebooting, same error message and logs.
Solved! Go to Solution.
2024-07-09 07:36 AM
Does the file exist?
If the build didn't complete there will be no output files to debug.
Watch for spaces or odd characters in files names and directory paths.
2024-07-09 07:36 AM
Does the file exist?
If the build didn't complete there will be no output files to debug.
Watch for spaces or odd characters in files names and directory paths.
2024-07-09 07:51 AM - edited 2024-07-09 08:19 AM
Do you have a folder name with a space in it; eg, "first example" or "first project" ... ?
🤔
Spaces in file names (including folder names) are best avoided!
https://www.avrfreaks.net/s/topic/a5C3l000000UXElEAO/t141557?comment=P-1144660
https://www.avrfreaks.net/s/topic/a5C3l000000UY8vEAG/t145039?comment=P-1182240
2024-07-09 08:59 AM
And the answer was odd characters :)) I have a "é" in my session name. Tried it in C:/ and it worked. Thank you very much !