STM32CubeIDE for Visual Studio Code (MCUs)

Ask questions on the STM32CubeIDE for Visual Studio Code extension. Find answers on a variety of topics, including build issues, debug functionalities, CMake project integration, and feature requests for CubeCLT installation.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can't build on VSCode

Hello, I have opened someone else's STM32 project in VSCode but I'm getting errors and I can't build. I think it has something to do with CMake, the extension is not asking me to generate a CMAKE config. Do I have to genereate a new project from IDE/...

hasansyr_0-1753450249011.png
hasansyr by Associate II
  • 656 Views
  • 7 replies
  • 1 kudos

Cube CLT install location on Mac

I am trying to get the SMT32 VS Code extension working and have installed the dependencies on my Mac. However, the extension doesn't seem to find Cube CLT.I ran into a couple issues during the install. First, it said that st-stm32cubeclt_1.17.0_23554...

btater by Associate
  • 4766 Views
  • 7 replies
  • 15 kudos

Resolved! Debugging under VS Code failed

Hi,I followed exactly the instructions of ST's youtube tutorial "Get started with STM32Cube for VS Code: from installation to debugging". (https://www.youtube.com/watch?v=aWMni01XGeI)Everything went perfect, the demo builds without problems.When it c...

dze.1 by Associate II
  • 1625 Views
  • 10 replies
  • 7 kudos

Resolved! Using time.h asserts

Hello,I am currently trying to convert my STM32CubeIDE (based on makefile) project to a STM32 VScode extension project based on CMake.Everything seemed to work smoothly until I was met with an issue calling the 'localtime' function from the standard ...

SharonVEC_0-1751357896942.png

Resolved! Trustzone debugging in VSCode

Hi, I am using Nucleo-WBA65RI and I have enabled trustzone. I generated the project using CubeMX and it generated a secure and a non-secure project. I have enabled the trustzone option byte and am able to run an example project with secure and non-se...

fa31 by Associate III
  • 849 Views
  • 6 replies
  • 0 kudos