2024-07-12 11:55 PM - edited 2024-07-13 12:23 AM
Using STM32 VS Code Extension 2.0.1 to create empty project for STM32C0116-DK board.
The generated startup_stm32c011f6ux.s file contains handlers in wrong (alphabetic ???) order:
g_pfnVectors:
.word _estack
.word Reset_Handler
.word NMI_Handler
.word HardFault_Handler
.word 0
.word 0
.word 0
.word 0
.word 0
.word 0
.word 0
.word SVC_Handler
.word 0
.word 0
.word PendSV_Handler
.word SysTick_Handler
.word ADC_IRQHandler /* ADC interrupt */
.word DMA1_Channel1_IRQHandler /* DMA1 channel 1 interrupt */
.word DMA1_Channel2_3_IRQHandler /* DMA1 channel 2 and 3 interrupts */
.word DMAMUX_IRQHandler /* DMAMUX interrupts */
.word EXTI0_1_IRQHandler /* EXTI line 0 and 1 interrupt */
.word EXTI2_3_IRQHandler /* EXTI line 2 and 3 interrupt */
.word EXTI4_5_IRQHandler /* EXTI line 4 and 5 interrupt */
.word I2C_IRQHandler /* global interrupt (combined with EXTI 23) */
.word RCC_IRQHandler /* RCC global interrupt */
.word RTC_IRQHandler /* RTC interrupts (EXTI lines 19) */
.word SPI_IRQHandler /* SPI/I2S global interrupt */
.word TIM1_BRK_UP_TRG_COM_IRQHandler /* TIM1 break, update, trigger and commutation interrupts */
.word TIM1_CC_IRQHandler /* TIM1 Capture Compare interrupt */
.word TIM3_IRQHandler /* TIM3 gloabal interrupt */
.word TIM14_IRQHandler /* TIM14 gloabal interrupt */
.word TIM16_IRQHandler /* TIM16 global interrupt */
.word TIM17_IRQHandler /* TIM17 global interrupt */
.word USART1_IRQHandler /* USART1 global interrupt (combined with EXTI 25) */
.word USART2_IRQHandler /* USART2 global interrupt (combined with EXTI 25) */
.word WWDG_IRQHandler /* Window watchdog interrupt */
.size g_pfnVectors, .-g_pfnVectors
wheras CubeMX 6.12 generates the correct one:
g_pfnVectors:
.word _estack
.word Reset_Handler
.word NMI_Handler
.word HardFault_Handler
.word 0
.word 0
.word 0
.word 0
.word 0
.word 0
.word 0
.word SVC_Handler
.word 0
.word 0
.word PendSV_Handler
.word SysTick_Handler
.word WWDG_IRQHandler /* Window WatchDog */
.word 0 /* reserved */
.word RTC_IRQHandler /* RTC through the EXTI line */
.word FLASH_IRQHandler /* FLASH */
.word RCC_IRQHandler /* RCC */
.word EXTI0_1_IRQHandler /* EXTI Line 0 and 1 */
.word EXTI2_3_IRQHandler /* EXTI Line 2 and 3 */
.word EXTI4_15_IRQHandler /* EXTI Line 4 to 15 */
.word 0 /* reserved */
.word DMA1_Channel1_IRQHandler /* DMA1 Channel 1 */
.word DMA1_Channel2_3_IRQHandler /* DMA1 Channel 2 and Channel 3 */
.word DMAMUX1_IRQHandler /* DMAMUX1 */
.word ADC1_IRQHandler /* ADC1 */
.word TIM1_BRK_UP_TRG_COM_IRQHandler /* TIM1 Break, Update, Trigger and Commutation */
.word TIM1_CC_IRQHandler /* TIM1 Capture Compare */
.word 0 /* reserved */
.word TIM3_IRQHandler /* TIM3 */
.word 0 /* reserved */
.word 0 /* reserved */
.word TIM14_IRQHandler /* TIM14 */
.word 0 /* reserved */
.word TIM16_IRQHandler /* TIM16 */
.word TIM17_IRQHandler /* TIM17 */
.word I2C1_IRQHandler /* I2C1 */
.word 0 /* reserved */
.word SPI1_IRQHandler /* SPI1 */
.word 0 /* reserved */
.word USART1_IRQHandler /* USART1 */
.word USART2_IRQHandler /* USART2 */
.word 0 /* reserved */
.word 0 /* reserved */
.word 0 /* reserved */
.size g_pfnVectors, .-g_pfnVectors
please fix
KnarfB
2024-07-13 4:00 PM