cancel
Showing results for 
Search instead for 
Did you mean: 

When was STM32WL5MOC module introduced, and can DASH7 protocol be implemented on it?

Amelie ACKERMANN
Community manager
Community manager

Shed some light on STM32WL5MOC module, when was it introduced, can we implement DASH7 protocol on it?

1 REPLY 1
Roman LUDIN
ST Employee

ST32WL5M was released January this year. we don't see a problem in using the Dash7 protocol with WL. The downside is that it is not officially supported by us, so the implementation/porting is up to the customer. From technical point of view we don't see a blocking point. Dash7 uses GFSK modulation, which is supported by the WL, so it is matter of software implementation.