How can we use one pin GPIO pin in both output mode and input mode?
How can we use one pin GPIO pin in both output mode and input mode?
How can we use one pin GPIO pin in both output mode and input mode?
What data formats (e.g. INT4/8/16, BF16, FP16) does the STM32MP2's NPU Accelerator support?
Can the dual GbE interfaces in the STM32MP133 be used as a TSN-switch?
When will STM32U031R6I6 go into production? What will be the 10-99pcs pricing per unit?
Can you drive display capabilities and the camera from the Cortex-M33 in the STM32MP2?
Is it possible to only run on the M33 with the Cortex-A in sleep mode on the STM32MP2, in order to keep a subset of functionality running but run on lower power?
On MP1, what is the fastest method communicate between A7 and M4?
Is the STM32WB5MMG going to evolve and propose more peripherals such as DAC's?
Which MCU is most suitable to interface LoRaWAN?
When will a nucleo board for the new stm32h7r will be released?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.