cancel
Showing results for 
Search instead for 
Did you mean: 

Why gets the SPI DMA configuration lost when re-opening *.ioc with CubeMX (STM32MP1)?

JMein.1
Associate III

My problem is, that on the one hand, the SPI3 configuration is lost after I close CubeMX.

  1. The assignment is lost to the M4 core (changed from A7 to M4 and after reopening, its again at A7. The changes have been saved and tried on different machines).
  2. If the assignment of the DMA streams for the peripherals has been done, after reopening CubeMx and *ioc file, the DMA streams differ or are completely lost.

 

So, what I am doing wrong here? Is there maybe another problem with the GPIO or whatever, which can lead to this unexpected behaviour? Or is this a known issue?

 

Thank you for the help.

 

Best regards,

Jan-Otto

10 REPLIES 10
PatrickF
ST Employee

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.