2024-11-14 11:47 PM - last edited on 2024-11-15 12:37 AM by mƎALLEm
I am trying to cross compile a simple helloworld.cpp program.
#include <iostream>
int main(int argc, char** argv)
{
std::cout << "Hello World" << std::endl;
return 0;
}
The makefile is
PROG = helloworld
SRCS = helloworld.cpp
CLEANFILES = $(PROG)
# Add / change option in CFLAGS and LDFLAGS
CFLAGS += -Wall $(shell pkg-config --cflags gtk+-3.0)
LDFLAGS += $(shell pkg-config --libs gtk+-3.0)
all: $(PROG)
$(PROG): $(SRCS)
$(CC) -o $@ $^ $(CFLAGS) $(LDFLAGS)
clean:
rm -f $(CLEANFILES) $(patsubst %.c,%.o, $(SRCS))
I have the developer package installed and I am able to compile the gtk_hello_world.c example just fine but If I try the above code it complies just fine but during the link it complains about std::cout and std::endl amoung other things related to iostream.
/home/lharris/STM32CubeIDE/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/libexec/arm-ostl-linux-gnueabi/gcc/arm-ostl-linux-gnueabi/12.3.0/ld: /tmp/ccoeJuW6.o: in function `main':
/home/lharris/Projects/HelloWorld1/helloworld.cpp:5: undefined reference to `std::cout'
and so on...
How can I compile a simple command line program using c++ conventions or is the needed library not in the cross development tool chain?
2024-11-15 12:05 AM
Hi @LHarr.1
have you looked to https://wiki.st.com/stm32mpu/wiki/Cross-compile_with_OpenSTLinux_SDK#Adding_Linux_user_space_applications ?
Regards.
2024-11-15 1:06 AM
I belive the answer is yes. I have followed the example gtk_hello_world.c and it runs just fine. I have also compiled a simple web server using the mongoose framework. So basic C functionality and C++ seem to work, just having a problem with using std::cout and it's ilk. I am suspecting that the support for std::cout in a console window is just not there.
2024-11-15 1:34 AM
I have done very little with C++ recently.
But wouldn't you need "another compiler", i.e. calling it as "g++" instead "gcc" ?
2024-11-22 9:07 PM
I go back and double check. I think I tried g++ as well but maybe not. If it works I’ll update this thread. Thanks for the suggestion and heads up.