2024-01-24 7:47 AM - edited 2024-01-24 7:48 AM
Dears,
I am able to compile Nx_WebServer demo. But when I try to run/debug it will halt.
I read all notes in NetXDuo/Nx_WebServer/readme.html - the last chapter "How to use it ?"
But I end on red line - unable load image - Where could be problem ?
I am able to compile and debug another aplication ftom STM32Cube_FW_MP13_V1.0 like UART, ADC examples withou error.
Error in final launch sequence:
Failed to execute MI command:
target extended-remote localhost:3333
Error message from debugger back end:
Remote communication error. Target disconnected.: (undocumented errno 10061).
Failed to execute MI command:
target extended-remote localhost:3333
Error message from debugger back end:
Remote communication error. Target disconnected.: (undocumented errno 10061).
Remote communication error. Target disconnected.: (undocumented errno 10061).
Console log:
Info : SWD DPIDR 0x6ba02477
Warn : target STM32MP135FAFx.ap1 examination failed
Warn : target STM32MP135FAFx.axi examination failed
Error: Could not initialize the APB-AP
Warn : target STM32MP135FAFx.cpu examination failed
Info : gdb port disabled
Info : gdb port disabled
Info : starting gdb server for STM32MP135FAFx.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Error: Target not examined yet
Error executing event gdb-attach on target STM32MP135FAFx.cpu:
Info : New GDB Connection: 1, Target STM32MP135FAFx.cpu, state: unknown
Error: Target STM32MP135FAFx.cpu not examined yet, refuse gdb connection 1!
Error: attempted 'gdb' connection rejected
shutdown command invoked
Best Regards
Radim
Solved! Go to Solution.
2024-02-13 1:34 AM - edited 2024-02-13 1:36 AM
Dear @DBELL.1
I have also tried to comment out creation of DHCPClient and appropriate callback
318: // ret = nx_dhcp_create(&DHCPClient, &IpInstance, "dhcp_client"); in app_netxduo.c
350: // ret = nx_ip_address_change_notify(&IpInstance, ip_address_change_notify_callback, NULL);
392: // ret = nx_dhcp_start(&DHCPClient);
Note: Also commented error handler for each statement "if (ret != NX_SUCCESS) {...}"
At end of initialization code in function UINT MX_NetXDuo_Init(VOID *memory_ptr) i put these lines:
ret = nx_ip_address_get(&IpInstance, &IpAddress, &NetMask);
PRINT_IP_ADDRESS(IpAddress);
PRINT_IP_ADDRESS(NetMask);
and it will report correct IP address...
So I suppose that IP was set and should be working. But application is still not working... What must I do to use static IP instead of using DHCP client ?
Best Regards
Radim
2024-02-13 2:02 AM
hello @ravo ,
This question seems to be a tricky one.
I asked some specialist people.
And I will post an answer as soon as I have it.
regards,
David
2024-02-13 3:26 AM - edited 2024-02-13 3:27 AM
Dear @DBELL.1 ,
thanks for your support.
And in meanwhile I browse source code again and found
line 398:
/* wait until an IP address is ready */
if(tx_semaphore_get(&Semaphore, TX_WAIT_FOREVER) != TX_SUCCESS)
{
Error_Handler();
}
When I remove waiting for this semaphore it will continue in App_Main_Thread_Entry and finish initialization of WebServer application.
So now it seems all works fine.
I will wait for your answer... if I need only these lines remove... or if there better way, some #define or etc.
Radim
2024-02-14 4:05 AM
Hello @ravo ,
I didn't receive any lowlight from expert about your modification.
So I guess, it's fine and you can go with it.
regards,
David
2024-02-20 11:06 PM
Dear @DBELL.1 ,
thanks for all.
Maybe there was some incompatibility with dhcpserver downloaded from https://www.dhcpserver.de/cms/download/
This will hang somewhere in initialization sequence.
Now with HW router with enabled DHCP or using STATIC IP address all works fine.
Regards
Radim