2024-01-24 7:47 AM - edited 2024-01-24 7:48 AM
Dears,
I am able to compile Nx_WebServer demo. But when I try to run/debug it will halt.
I read all notes in NetXDuo/Nx_WebServer/readme.html - the last chapter "How to use it ?"
But I end on red line - unable load image - Where could be problem ?
I am able to compile and debug another aplication ftom STM32Cube_FW_MP13_V1.0 like UART, ADC examples withou error.
Error in final launch sequence:
Failed to execute MI command:
target extended-remote localhost:3333
Error message from debugger back end:
Remote communication error. Target disconnected.: (undocumented errno 10061).
Failed to execute MI command:
target extended-remote localhost:3333
Error message from debugger back end:
Remote communication error. Target disconnected.: (undocumented errno 10061).
Remote communication error. Target disconnected.: (undocumented errno 10061).
Console log:
Info : SWD DPIDR 0x6ba02477
Warn : target STM32MP135FAFx.ap1 examination failed
Warn : target STM32MP135FAFx.axi examination failed
Error: Could not initialize the APB-AP
Warn : target STM32MP135FAFx.cpu examination failed
Info : gdb port disabled
Info : gdb port disabled
Info : starting gdb server for STM32MP135FAFx.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Error: Target not examined yet
Error executing event gdb-attach on target STM32MP135FAFx.cpu:
Info : New GDB Connection: 1, Target STM32MP135FAFx.cpu, state: unknown
Error: Target STM32MP135FAFx.cpu not examined yet, refuse gdb connection 1!
Error: attempted 'gdb' connection rejected
shutdown command invoked
Best Regards
Radim
Solved! Go to Solution.
2024-02-13 3:26 AM - edited 2024-02-13 3:27 AM
Dear @DBELL.1 ,
thanks for your support.
And in meanwhile I browse source code again and found
line 398:
/* wait until an IP address is ready */
if(tx_semaphore_get(&Semaphore, TX_WAIT_FOREVER) != TX_SUCCESS)
{
Error_Handler();
}
When I remove waiting for this semaphore it will continue in App_Main_Thread_Entry and finish initialization of WebServer application.
So now it seems all works fine.
I will wait for your answer... if I need only these lines remove... or if there better way, some #define or etc.
Radim
2024-01-25 9:48 AM
Dear @ravo
I do not reproduce this error at my end in running this particular example after following the readme file.
This typical error msg usually indicates that
1- you haven't run the DDR init example prior running the NX_webserver project
2. you haven't changed the NX_webserver/debug properties as mentioned in the readme file (please remove “monitor reset” line )
Board boot pins must be set in "Engineering boot mode" But you said you were already familiar with other HAL examples so I don't think this was your issue.
Best Regards
Olivier
2024-01-25 8:34 PM - edited 2024-01-25 11:27 PM
Dear @OlivierK ,
Thanks for answer.
As I wrote earlier I have already run DDR Init, and monitor reset lin in debug prop in startup section was removed. But how to verify if it is running ok?
Maybe I do something wrong here:
Rebuild all files and load your image into target memory
I am doing it using STM32CubeIde with Debug command, is it ok?
Regards Radim
2024-01-26 12:53 AM
Small update,
I have looked that blue led is blinking (after DDR_Init - but only when it is running in DEBUG mode, when RUN then nothing...)
Then I am able to start DEBUG for NETX Duo application... But then it will show warning...
When I push Resume button, then it will start...
I got info in UART that project is running. But unable to continue...
When stop and restart debug once more it will never send data to UART...
May I doing still something wrong ?
Regards
Radim
2024-01-26 1:34 AM
Hi @ravo
Yes, CubeIDE projects are made to be debugged directly in Engineering mode by plugging a stlink usb cable,
I use the bug button to enter debug:
It means you need to run the DDR_init example first, if properly done you should see the blue led toggling (DK-board) indicating the DDR is properly initialized. Once there, you should quit the DDR init project without resetting the board.
Regarding the projet build itself, there is nothing to change it works as is. If you want to enable the Nx_WebServer_A7 debug symbol you can modify :
Regards,
Olivier
2024-01-26 2:40 AM
Dear @OlivierK
thanks for your comments.
Really I must do "Rebuild and run DDR_Init example to initialize the DDR memory" every time prior to start new debug session for Nx_WebServer application ?
I only receive "Nx_Webserver application started.." in UART terminal
nothing else...
So I tried adding more debug prints... and I see that all initialization is done successfully.
Can I define specific IP address instead using DHCP ?
Best regards
Radim
2024-01-29 6:47 AM
Second update.
I found how change to static IP:
In file Applications/NetXDuo/Nx_WebServer/NetXDuo/App/app_netxduo.c
line 175:
ret = nx_ip_create(&IpInstance, "NetX IP Instance 0", STATIC_IP_ADDRESS, MASK_IP_ADDRESS, &EthPool, nx_stm32_eth_driver,
pointer, 2 * DEFAULT_MEMORY_SIZE, DEFAULT_PRIORITY);
when define:
#define STATIC_IP_ADDRESS IP_ADDRESS(192,168,0,2)
#define MASK_IP_ADDRESS IP_ADDRESS(255,255,255,0)
Then when I try ping board it answer correctly. So application is running and it is connected to network
But still no mor logs... is it normal ?
I copy content of ..\Applications\NetXDuo\Nx_WebServer\Web_Content\ to root of microSD formated as FAT.
But I only get ping response, unable to get running web server on http://192.168.0.2/
I have read readme.html once more... but I can't find where is the error.
Thanks in advance for your help.
Regards Radim
2024-02-12 8:22 AM
Hello @ravo ,
It seems you have the same DHCP server problem to provide the address as the other post.
https://community.st.com/t5/stm32cubeide-mpus/nx-iperf-a7-unable-run-tcp-test-both-client-server-and-udp/td-p/634463
Did it work well now?
regards,
David
2024-02-12 10:31 PM
Dear @DBELL.1
Yes you are correct, now the application is running normally. But I have some notes:
(1) When opening http://IP@/about.html is OK as it was written in readme.html. But there should be better to retarget from http://IP@/ or usage index.html for better usage.
(2) And for last How to setup NetXDuo to use static IP address ? As I wrote in previous post. I am able to start using:
ret = nx_ip_create(&IpInstance, "NetX IP Instance 0", STATIC_IP_ADDRESS, MASK_IP_ADDRESS, &EthPool, nx_stm32_eth_driver,
pointer, 2 * DEFAULT_MEMORY_SIZE, DEFAULT_PRIORITY);
when define:
#define STATIC_IP_ADDRESS IP_ADDRESS(192,168,0,2)
#define MASK_IP_ADDRESS IP_ADDRESS(255,255,255,0)
But then NetXDuo application did not work correctly (only ping response)
What could be here wrong...
Best Regards
Radim
2024-02-13 1:01 AM
Hello @ravo ,
Further in the code, in the same function, there are:
ret = nx_dhcp_create(&DHCPClient, &IpInstance, "dhcp_client");
and
ret = nx_ip_address_change_notify(&IpInstance, ip_address_change_notify_callback, NULL);
and in App_Main_Thread_Entry():
ret = nx_dhcp_start(&DHCPClient);
where the address is set.
That's why your modification shouldn't be taken into account.
regards
David