cancel
Showing results for 
Search instead for 
Did you mean: 

[MacOS] Can't open or import .ioc file using CubeMX

f4_kiddo
Associate II

Hi,

currently I can't open any .ioc file which hasn't been previously created with my computer.

There's no problem if I open an .ioc file inside CubeIDE, but, when I want to use VS Code I need to open the .ioc file using just CubeMX.

If I open an .ioc file with CubeMX, the program brings me the startup page. Whether I try to load a project directly from CubeMX, I can't navigate through the folders because, even in the Desktop folder the file navigator shows me an empty space.

Does anyone have my same problem, with MacOS?

0693W00000LvxMiQAJ.png

1 ACCEPTED SOLUTION

Accepted Solutions
Aymen CHAKROUN
ST Employee

Hi @f4_kiddo​,

Can you follow the solution described in this post ?

STM32CubeMX 6.4.0 doesn't interact nicely with MacOS 12.1 (Monterey)

Let me know the result.

Regards,

Aymen.

View solution in original post

4 REPLIES 4
Aymen CHAKROUN
ST Employee

Hi @f4_kiddo​,

Can you follow the solution described in this post ?

STM32CubeMX 6.4.0 doesn't interact nicely with MacOS 12.1 (Monterey)

Let me know the result.

Regards,

Aymen.

Thank you so much!

Now it's working fine :beaming_face_with_smiling_eyes:

RMora.4
Associate III

I was having the same problem and this solution worked for me. Thank you.

Although I will say that this shouldn't be an issue that we should be struggling with. I don't remember this being an issue when I installed an earlier version of CubeMX.

Intended a reply on my initial comment

"I was having the same problem and this solution worked for me. Thank you. 

Although I will say that this shouldn't be an issue that we should be struggling with. I don't remember this being an issue when I installed an earlier version of CubeMX."