2019-09-19 7:16 AM
I can't connect to my STM32MP157 evalaution board. I have installed required libraries as decribed in the tutorial: https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Package 5.1 Installing the STM32CubeProgrammer tool. However I get the following error:
===== DFU Interface =====
STM32_Programmer_CLI: symbol lookup error: STM32_Programmer_CLI: undefined symbol: libusb_get_port_number
2019-10-01 7:34 AM
Hi @KZura
I suspect a problem with the USB/DFU driver.
Did you go through 5.2 Preparing the USB serial link for flashing also ?
Are you working with Windows or Linux host machine ?
Hope it help
Olivier
2019-10-01 7:49 AM
Hi OlivierG, thanks for your reply.
Yes I have went through 5.2 Preparing the USB serial link for flashing step.
I am using Linux 16.04 host machine.
What else could I provide to track this issue down?
Thanks!
Chris
2019-10-01 8:02 AM
Can you share the full command you execute
Thx
Olivier
2020-05-18 1:30 PM
Not the original poster, but I have the exact same issue.
Command is "STM32_Programmer_CLI -l usb"
Output is:
-------------------------------------------------------------------
STM32CubeProgrammer v2.4.0
-------------------------------------------------------------------
===== DFU Interface =====
STM32_Programmer_CLI: symbol lookup error: STM32_Programmer_CLI: undefined symbol: libusb_get_port_number