2021-07-13 4:58 AM
If I want to fully erase eval board STM32MP15F and then re-populate it back to its original out-of-the-box state. Is it enough to upload the flash layout from:
en.FLASH-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31.tar_v3.0\stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31\images\stm32mp1\flashlayout_st-image-weston\trusted
and reboot the board? Or are there any other steps I should follow?
Best regards, Arnas
Solved! Go to Solution.
2021-07-13 8:12 AM
Hi,
for STM32MP family, we did not talk about 'chip' erase (as for MCUs with embedded Flash) but 'Flash' erase (Flash is external to the chip).
It is usually not needed using the provided Flashlayout.
Anyway, if you really want to erase the memory before flashing, one way to acheive this is to replace the 'P' options in the existing flashlayout by 'PD'.
e.g. for EV1 board, Trusted Starter Package on SD-Card:
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157f-ev1-usb.stm32
- 0x03 fip-boot Binary none 0x0 fip/fip-stm32mp157f-ev1-trusted.bin
PD 0x04 fsbl1 Binary mmc0 0x00004400 arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32
PD 0x05 fsbl2 Binary mmc0 0x00044400 arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32
PD 0x06 fip Binary mmc0 0x00084400 fip/fip-stm32mp157f-ev1-trusted.bin
PD 0x10 boot System mmc0 0x00484400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4
PD 0x11 vendorfs FileSystem mmc0 0x04484400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
PD 0x12 rootfs FileSystem mmc0 0x05484400 st-image-weston-openstlinux-weston-stm32mp1.ext4
PD 0x13 userfs FileSystem mmc0 0x33E84400 st-image-userfs-openstlinux-weston-stm32mp1.ext4
But as Flash erasing take long time (especially the big userfs partition), in order to avoid timeout with CubeProgrammer GUI (fixed timeout), you should use STM32_Programmer_CLI (same functionality but on command line) and add '-tm 120000' to increase the timeout to allow the erase sequence to complete (here 120 seconds is enough for a 16GB SD-Card).
e.g. on Windows 10, for EV1 board, Trusted Starter Package on SD-Card:
STM32_Programmer_CLI.exe -c port=usb1 -w flashlayout_st-image-weston\trusted\FlashLayout_sdcard_stm32mp157f-ev1-trusted.tsv -tm 120000
Regards.
2021-07-13 5:12 AM
Hi,
to Flash Starter Package to STM32MP157F-DK2 board, see https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Let's_start/Populate_the_target_and_boot_the_image
(similarly for STM32MP157F-EV1 board: https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-EV1/Let%27s_start/Populate_the_target_and_boot_the_image_
Regards.
2021-07-13 5:38 AM
Thanks, Patrick, my question was a bit dummy one, i just was confused, why can I upload both the flashlayout_st-image-weston/trusted AND flashlayout_st-image-weston/optee ? Does the /trusted file content will not set everything ?
Thanks!
2021-07-13 6:29 AM
Hi,
On a product, usually only one Flashlayout is used. All provided Flashlayout flash everything to have a working Starter Package.
I agree that during evaluations, you could try one flashlayout and later another flashlayout.
I cannot guarantee that there is no side effect using many different flashlayout in sequence, but I think it has been designed to work in such a way (e.g. there is a PD to fully erase FIP partition before flashing, see https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#SD_card_with_FIP).
Regards,
2021-07-13 6:42 AM
Thanks, Patrick,
If i got it correctly, when using the STM32CubeProgrammer we should always follow:
step 1: full chip erase
step 2: use ***/flashlayout_st-image-weston/trusted directory to pin point the flash layout
There should be no issues.
2021-07-13 7:50 AM
ahh also small issue the STM32CubeProgrammer does NOT support full chip erase for smt32mp1 familly
2021-07-13 8:12 AM
Hi,
for STM32MP family, we did not talk about 'chip' erase (as for MCUs with embedded Flash) but 'Flash' erase (Flash is external to the chip).
It is usually not needed using the provided Flashlayout.
Anyway, if you really want to erase the memory before flashing, one way to acheive this is to replace the 'P' options in the existing flashlayout by 'PD'.
e.g. for EV1 board, Trusted Starter Package on SD-Card:
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157f-ev1-usb.stm32
- 0x03 fip-boot Binary none 0x0 fip/fip-stm32mp157f-ev1-trusted.bin
PD 0x04 fsbl1 Binary mmc0 0x00004400 arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32
PD 0x05 fsbl2 Binary mmc0 0x00044400 arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32
PD 0x06 fip Binary mmc0 0x00084400 fip/fip-stm32mp157f-ev1-trusted.bin
PD 0x10 boot System mmc0 0x00484400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4
PD 0x11 vendorfs FileSystem mmc0 0x04484400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
PD 0x12 rootfs FileSystem mmc0 0x05484400 st-image-weston-openstlinux-weston-stm32mp1.ext4
PD 0x13 userfs FileSystem mmc0 0x33E84400 st-image-userfs-openstlinux-weston-stm32mp1.ext4
But as Flash erasing take long time (especially the big userfs partition), in order to avoid timeout with CubeProgrammer GUI (fixed timeout), you should use STM32_Programmer_CLI (same functionality but on command line) and add '-tm 120000' to increase the timeout to allow the erase sequence to complete (here 120 seconds is enough for a 16GB SD-Card).
e.g. on Windows 10, for EV1 board, Trusted Starter Package on SD-Card:
STM32_Programmer_CLI.exe -c port=usb1 -w flashlayout_st-image-weston\trusted\FlashLayout_sdcard_stm32mp157f-ev1-trusted.tsv -tm 120000
Regards.
2021-07-15 4:42 AM
Thanks, will try that!