cancel
Showing results for 
Search instead for 
Did you mean: 

what is the maximum EMMC capacity supported

Wjian.1
Associate II

Hi:

I would like to ask what is the maximum EMMC capacity supported by stm32mp157A chip.Can you give me some advice.eg:128g

2 REPLIES 2
PatrickF
ST Employee

Hello,

I think the limit is not given by STM32MP15x hardware nor boot mechanism (which is in ROM), but rather by the Linux filesystem support.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Ok, Got it. Thanks for your quick reply