2021-04-07 1:31 AM
We are using SoM MYC-YA157C from MYIR with STM32MP1 onboard. MYIR creates pretty device-tree hierarchy, which is handy for update. CubeMX creates partial single device tree file. I would like to merge some of it parts (pinmxing, for instance) with MYIR device tree into resulting DTS file. What is a proper way for doing it ?
PS. Xilinx provides system-user.dtsi file which is included AFTER all system DTSI`s in such way that it adds or overrides contents of system DTSI while merging into final DTS file. It is very convenient. Does STM provide similar capabilities ?
2021-04-09 7:20 AM
Hi @mishuk
Did you have a look to https://wiki.st.com/stm32mpu/wiki/STM32MP15_device_tree ( pay attention current version fit with latest V3.0 release previous version are available as archive https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/Main_Page https://wiki.st.com/stm32mpu-ecosystem-v2/wiki/Main_Page)
It explain device-tree hierarchy of our offer either from upstreamed source or from CubeMX.
For ST the latest level where you can adds/override contents is the "board" dts level.
I'm not aware of MYIR device-tree hierarchy but I guess might be same philosophy.
Hope it help
Olivier
2021-04-12 2:54 AM
Thank you for your explanation. The link you have provided is helpful. Does Cube-MX generate GPIO specific pinctlr node ? I can`t find GPIO pinctrl`s in DTS file from CubeMX . I2C, SPI pinctrl`s seem OK.
2021-04-16 7:04 AM
I still can`t find GPIO pinctrls in DTS file from CubeMX. Why CubeMX doesn`t generate them ?
2021-04-19 5:01 AM
Hi @mishuk
CubeMX only handle GPIO pinctrl related to IPs. ( I2C, SPI)
For other GPIO configuration you have to manage it your own following https://wiki.st.com/stm32mpu/wiki/GPIO_device_tree_configuration
Hope it help
Olivier
2021-04-19 6:23 AM
Would you be so kind for providing step-by-step manual for setting "free" (NOT related to IPs) GPIOs in device-tree ?