cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to download SDK for stm32mp1

JSpra
Associate III

Hi,

While following the example at https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package#Updating_the_kernel_device_tree, I'm running into problems downloading the SDK.

The link provided from instructions below, always downloads the "SOURCES" tar not the "SDK".

Developer package:

  • the SDK toolchain, provided within the en.SDK-x86_64-stm32mp1-openstlinux-<YY>-<MM>-<DD>.tar.xz file (download it from st.com)

I have tried searching for the SDK at other places on your web-site, all results bring back the

en.SOURCES-stm32mp1-openstlinux-5-4-dunfell-mp1-20-06-24.tar.xz not the SDK

Could someone please verify this issue and point me to where I can get the SDK.

Thanks in advance!

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
ArmandG
ST Employee

Hi @JSpra​ ,

In case you are still stuck with it, you need to click on Yocto_SDK link and not STM32MP1DeveloperPackage.

Regards,

Armand

JSpra
Associate III

Well, I was running down a device tree compile issue using Yocto SDK, thought I would see if I got same results using STM's suggestion for device tree compile.

Good suggestion though, thanks for the reply!

ArmandG
ST Employee

Hi @JSpra​ ,

For the device tree compile issue using Yocto SDK I suggest you to create another topic about this, maybe one can help you.

Armand