2019-04-28 4:36 PM
Inorder to build a developer package, i am following the link : https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package
I am not able to apply the patch to the linux kernel.
when i try to apply patches the terminal is stuck
STM32MP157c-DK2
Solved! Go to Solution.
2019-04-29 2:39 AM
I looks you are not in the correct directory to apply the patch.
you should be in (..)sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.9
and use this command : $for p in `ls -1 ../*.patch`; do patch -p1 < $p; done
Also, are you in shell compatible with SDK cross-compilation ?
If not please do this before any other command :
$source [Developer_Package_Path]/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi
Hope it help
Olivier
2019-04-29 12:37 AM
Hi @Vthul
In order I can help can you please confirm you are at step "5.2.2 Building and deploying the Linux kernel for the first time" of the wiki.
You refer to the README.HOW_TO.txt ?
Can you please share exactly the steps you have followed ? Are you doing installation in build directory or in source path ?
Can you share a screen copy of the command freezing the terminal ?
Thx
Olivier
2019-04-29 2:05 AM
Hi @Community member ,
Thanks for your reply.
In order I can help can you please confirm you are at step "5.2.2 Building and deploying the Linux kernel for the first time" of the wiki.
You refer to the README.HOW_TO.txt ? ---Yes
I am following the README.HOW_TO.txt.
I have extracted the Linux files and obtained the patches.
So the step is to apply the patches before compiling if i am not wrong.
To apply patches, i am doing this
So in 3rd point ---> $> for p in `ls -1 <path to patch>/*.patch`; do patch -p1 < $p; done
and i get as in above screen shot
<path to patch> i am already in current working directory as that of the linux Kernel
Regards,
Viveknath
2019-04-29 2:39 AM
I looks you are not in the correct directory to apply the patch.
you should be in (..)sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.9
and use this command : $for p in `ls -1 ../*.patch`; do patch -p1 < $p; done
Also, are you in shell compatible with SDK cross-compilation ?
If not please do this before any other command :
$source [Developer_Package_Path]/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi
Hope it help
Olivier
2019-04-29 2:49 AM
Hello ,
Also, are you in shell compatible with SDK cross-compilation ? -> yes
and use this command : $for p in `ls -1 ../*.patch`; do patch -p1 < $p; done - this worked .
thanks a lot