cancel
Showing results for 
Search instead for 
Did you mean: 

enable M4 log on STM32MP1 ( STM32MP157-DK2 dev kit)

OJohn
Associate

Hello,

I am able to compile the M4 examples and it looks as though they run as expected ( I can see the log trace on the A7 side from the linux console). I would like to examine the log trace from the M4 side also as I would like to modify some of these examples for further use. In the OpenAMP_TTY_echo example (main.c) are the following lines

 log_info("Cortex-M4 boot successful with STM32Cube FW version: v%ld.%ld.%ld \r\n",

                                           ((HAL_GetHalVersion() >> 24) & 0x000000FF),

                                           ((HAL_GetHalVersion() >> 16) & 0x000000FF),

                                           ((HAL_GetHalVersion() >> 8) & 0x000000FF));

I was curious as to how I can enable these lines. Do I need to enable putc associated with one of the UART instances or ..

Basically just want to know how I can have console functionality on the M4 side also

Thanks

Victor

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hello, I'm not 100% sure of the answer,

Need to define __LOG_TRACE_IO_ in M4 preprocessor directives

Traces are then available under Linux using e.g. cat /sys/kernel/debug/remoteproc/remoteproc0/trace0

(see Linux_remoteproc_framework_overview#How_to_trace_and_debug_the_framework)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

View solution in original post

1 REPLY 1
PatrickF
ST Employee

Hello, I'm not 100% sure of the answer,

Need to define __LOG_TRACE_IO_ in M4 preprocessor directives

Traces are then available under Linux using e.g. cat /sys/kernel/debug/remoteproc/remoteproc0/trace0

(see Linux_remoteproc_framework_overview#How_to_trace_and_debug_the_framework)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here