2023-06-25 6:48 AM
Hello,
I've been trying to boot my STM32MP157F-EV1 evaluation board from the SD card but I get the result that is shown in the image when using minicom. I used to work on the board for a long time with no problem, but recently I tried booting it again and this happened. I'm not sure if it's a hardware or a software problem. I made sure that the SD card is inserted correctly and that the boot switch configuration is set for SD card. I tried ping and ssh commands with the IP address but no connection is visible.
Is there a way to fix this problem? Any help would be appreciated.
2023-06-25 11:27 PM
Hi @Yamir.1
Did you try flashing again the Latest Starter Package on a different SD-Card ?
Regards.
2023-06-27 8:57 AM
Hello
I tried using a different SD card but when I try to populate it by following the instructions in the link you provided the STM32CubeProgrammer fails to detect the USB port when I press the refresh button, which is the same result when doing it with the previous SD card.
I made sure that the boot switches are in the right position and to reset the board. I also made sure that I have both the OTG and ST-Link USB ports connected to my PC and that their LED indicators are on.
Best Regards,
2023-06-28 2:23 AM
HI @Yamir.1
To flash the board, please try BOOT pins = 0b0000 (all switch on 'ON' side).
Is the red led (LD2) stop toggling when you connect a PC on CN16 (motherboard) ?
Could you try connecting only STLINK (CN4 of Dautherboard) and dump ROM boot traces using https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_trace_analyzer ?
Regards
2023-07-01 6:26 AM
Hello,
Yes, the red LED does stop toggling when I connect my PC to CN16 with that BOOT pin configuration that you gave. As for dumping ROM boot traces I followed the instructions and I got the following result in my console.
However, I am still unable to connect to my board.
Best Regards,
2023-07-19 1:14 AM
Hi @Yamir.1 ,
To get bootrom traces decoded, you should then process the trace.bin with the python script provided in https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_trace_analyzer#On_STM32MP15x_lines_2
save the script provided in a rom_trace_analyzer.py file, then:
python rom_trace_analyzer.py traces.bin
Regards