Skip to main content
Visitor II
July 20, 2023
Question

STM32MP151 in USB/UART boot mode after reboot

  • July 20, 2023
  • 1 reply
  • 1744 views

Hello,

We are using the STM32MP151 custom board microprocessor with an external flash memory (emmc). At start-up the board and linux boot correctly, but when reboot it, the board keeps in uart/usb boot loader mode and doesn't boot. It happen also when we reboot with a push button in rst pin and with software reboot.

When we reboot in software reboot, the last traces we get are:

Ma_mh1_0-1689848613566.png

Could you help us? Thanks.

Regards.

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
July 20, 2023

HI @Ma_mh1 

Maybe you are using power discrete (no STPMIC1) and you do not connect correctly the NRST_CORE pin (see AN5031 or ES0438)

If not the root cause, dump and analyze ROM boot traces using STLINK : https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_trace_analyzer ?

Regards.

 

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent