2024-10-29 02:17 PM - last edited on 2024-11-01 07:12 AM by Andrew Neil
I'm very proud of STM32MP1 and I want to continue to learn more about the STM32MP products.
So, I'm planning to create another single board computer such as the open source project STM32-Computer. My next project will be STM64-Computer, which will use STM32MP257.
I have some questions that are refering to the STM32MP2 series.
Thank you!
2024-11-23 07:16 AM
> I understand that MP2 is to slow for youtube.
I would say this statement is too broad.
Most probably too slow for YT at 720p or 1080i resolution. Systems designed for this purpose use multiple symmetrical cores - usually four of eight - and GPUs to achieve the required throughput. Which comes at a cost, in power consumption and complexity. Factors which do matter in a lot of applications.
2024-11-24 06:41 AM
Is it possible to put all the YT consumtion on the GPU instead?
The STM32MP2 have two cores and one GPU.