2023-07-25 3:19 AM
Hi,
I have a problem with hanging up my board occasionally when an issue from the console reboot.
I read about and the internet says this is a problem with the EMMC memory's power cycle.
So I followed by a link
but still, after a few reboots my board stacked.
My final message from the console is as follows
[ OK ] Stopped Create Static Device Nodes in /dev.
[ OK ] Reached target System Shutdown.
[ OK ] Reached target Late Shutdown Services.
[ OK ] Finished System Reboot.
[ OK ] Reached target System Reboot.
[ 32.494373] watchdog: watchdog0: watchdog did not stop!
[ 32.522678] systemd-shutdown[1]: Using hardware watchdog 'STM32 Independent 0
[ 32.533457] systemd-shutdown[1]: Watchdog running with a timeout of 2min.
[ 32.559399] systemd-shutdown[1]: Syncing filesystems and block devices.
[ 32.687090] systemd-shutdown[1]: Sending SIGTERM to remaining processes...
[ 32.713669] systemd-journald[685]: Received SIGTERM from PID 1 (systemd-shut.
[ 32.738780] systemd-shutdown[1]: Sending SIGKILL to remaining processes...
[ 32.764536] systemd-shutdown[1]: Unmounting file systems.
[ 32.774792] [1459]: Remounting '/' read-only with options 'n/a'.
[ 32.798594] EXT4-fs (mmcblk1p8): re-mounted. Opts: (null). Quota mode: disab.
[ 32.825938] systemd-shutdown[1]: All filesystems unmounted.
[ 32.830174] systemd-shutdown[1]: Deactivating swaps.
[ 32.835585] systemd-shutdown[1]: All swaps deactivated.
[ 32.840200] systemd-shutdown[1]: Detaching loop devices.
[ 32.854929] systemd-shutdown[1]: All loop devices detached.
[ 32.859153] systemd-shutdown[1]: Stopping MD devices.
[ 32.865032] systemd-shutdown[1]: All MD devices stopped.
[ 32.869346] systemd-shutdown[1]: Detaching DM devices.
[ 32.875192] systemd-shutdown[1]: All DM devices detached.
[ 32.879905] systemd-shutdown[1]: All filesystems, swaps, loop devices, MD de.
[ 32.924796] systemd-shutdown[1]: Syncing filesystems and block devices.
[ 32.930334] systemd-shutdown[1]: Rebooting.
[ 33.167515] reboot: Restarting system
INFO: PSCI Power Domain Map:
INFO: Domain Node : Level 1, parent_node -1, State ON (0x0)
INFO: Domain Node : Level 0, parent_node 0, State ON (0x0)
INFO: CPU Node : MPID 0x0, parent_node 0, State ON (0x0)
INFO: CPU Node : MPID 0x1, parent_node 0, State ON (0x0)
How to resolve this issue?
Thanks
BR
Michał
Solved! Go to Solution.
2023-07-25 6:09 AM
Hi @MWoło.2
this might come up from a know limitation, not linked to eMMC.
In case your board did not use STPMIC1 for supply (which issue a power cycle on VDDCORE in case of reset), you should connect NRST to NRST_CORE with a 1nF capacitor as listed in ES0438 "Incorrect reset of glitch-free kernel clock switch" or AN5031 "Discrete supplies example 3.3 V I/Os with DDR3L"
Regards,
2023-07-25 6:09 AM
Hi @MWoło.2
this might come up from a know limitation, not linked to eMMC.
In case your board did not use STPMIC1 for supply (which issue a power cycle on VDDCORE in case of reset), you should connect NRST to NRST_CORE with a 1nF capacitor as listed in ES0438 "Incorrect reset of glitch-free kernel clock switch" or AN5031 "Discrete supplies example 3.3 V I/Os with DDR3L"
Regards,
2023-07-26 1:53 PM
Hi Patrick,
it's working. I take care of everything else without connecting through the cap that two mentioned NRST.
Thanks a lot, the topic can be closed.
Best Regards
Michał