2019-11-28 3:02 AM
I am trying to flash a 32gb sd card with stlinux for STM32MP157C-DK2 using the guide at https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Let%27s_start/Populate_the_target_and_boot_the_image
The SD card that came with the kit boot perfectly, I just want to flash another sd card.
I am using Ubuntu 16.04 LTS on my laptop
details about my STM32MP157C-DK2
Serial number(below pcb) : DK32MP157C2$AU1
These are the commands I ran and the output I got on console :
$ STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 002900333338510939303435
FW version : 0x0110
Device ID : 0x0500
Device name : STM32MPxxx
Device type : MPU
Device CPU : Cortex-A7
Start Embedded Flashing service
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32
File : tf-a-stm32mp157c-dk2-trusted.stm32
Size : 245364 Bytes
Partition ID : 0x01
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.666
RUNNING Program ...
PartID: :0x01
Start operation done successfully at partition 0x01
Flashlayout Programming ...
[==================================================] 100%
Running Flashlayout Partition ...
Flashlayout partition started successfully
Memory Programming ...
Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32
File : u-boot-stm32mp157c-dk2-trusted.stm32
Size : 805514 Bytes
Partition ID : 0x03
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.989
RUNNING Program ...
PartID: :0x03
reconnecting the device ...
Error: unable to reconnect the target device: time out expired
Error: Start operation failed at partition 0x03
Error: TSV flashing service failed
Solved! Go to Solution.
2019-11-29 4:58 AM
You use a supply which is not USB Type-C compliant !
Error is issued because uBoot does not detect the right CC lines levels as required by the USB standard. So boot process stop (This is a SW choice for our DK2 started package, you are free to modify/rebuilt uBoot to ignore this).
Please have a look to this post which list some tested supplies: https://community.st.com/s/question/0D50X0000Bftr1ySQA/power-supply-for-stm32mp157cdk2
2019-11-29 5:29 AM
Thanks for the info,
Can you provide me with some resources related to development using the DK2 Kit, I want build a user interface for a project.
I am familiar with MCUs but when using an MPU such as in the DK2, how would one make a solution where when the device is booted up, a user interface opens automatically for some HMI and the user can interact using the screen, I also want it to be able to connect to wifi. How can one build something like this using the DK2.
Please help me.
Thanks in advance.
2019-11-29 5:35 AM
I was thinking about writing a GTK3 application and sending it to the DK2, but how would connect to wifi and send API requests to server.
2019-11-29 6:17 AM
Yes it is a good idea to use GTK, you will find many help from the community and some basic samples applications developed by ST (GTK + Python) on the starter packages.